SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
In HDQ mode, the firmware does not require the host to create an initialization pulse to the slave. However, the slave can be reset by using an initialization pulse (also referred to as a break pulse). The initialization pulse is generated by setting the HDQ_CTRL_STATUS[2] INITIALIZATION bit and then setting the HDQ_CTRL_STATUS[4] GO bit. The slave does not respond with a presence pulse as it does in the 1-Wire protocol.
The HDQ is a command-based protocol in which the host sends a command byte to the slave. The command directs the slave either to store the next eight bits of data received to a register specified by the command byte (write operation) or to output the eight bits of data from a register specified by the command byte (read operation). The master implementation is a simple byte engine. Sending of the ID, command/address, and data is controlled by firmware. The master engine provides only a single HDQ_TX_DATA register.
The command and data bytes consist of a stream of eight bits with a maximum transmission rate of 5 Kbps. The least-significant bit (LSB) of a command or data byte is transmitted first. If a communication time-out occurs between the host and the slave (for example, if the host waits longer than the specified time for the slave to respond, or if this is the first access command), then the host must send an initialization pulse (BREAK) before sending the command again.
The slave detects a break when the HDQ pin is driven to a logic-low state for a specified break time t(B) or greater. The HDQ pin then returns to its normal ready-high logic state for a specified break-recovery time t(BR). The slave is then ready for a command from the host processor. Figure 24-30 shows this behavior.
An interrupt condition indicates a TX-complete, an RX-complete, or a time-out condition. Reading the interrupt status register clears all interrupt conditions. Only one interrupt signal is sent to the microcontroller, and only one overall mask bit can enable or disable the interrupt. The interrupt conditions cannot be individually masked.
Figure 24-30 HDQ Break-Pulse Timing Diagram