SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Figure 8-55 provides an illustration of different actions and events of interest during an interrupt processing. In this case, both INT4 and INT5 were asserted simultaneously, INT4 was selected as the winner and was taken after few cycles when all enable conditions (CSR[0]GIE, IER[1]NMIE, IER[n]) were met.
Note that the CPU entity signals/registers are shown in bold font; internal (and sometimes just conceptual) signals are shown in normal font.
The conceptual signal “Interrupt Accept” shows when a particular interrupt (in this case, INT4) is accepted to be taken next. This is generated by considering that all set bits of IFR, the interrupt priority, the enable conditions, and a safe cycle boundary within the CPU, where accepting an interrupt is safe.
The conceptual signal “Interrupt Taken” shows when a particular interrupt (in this case, INT4) is actually taken. The actions corresponding to an interrupt processing (IST access, context save, etc.) starts to take place within the CPU after this condition is achieved.
The delay between ‘Interrupt Accept’ and ‘Interrupt Taken’ is due to pending memory transaction on CPU instruction and data interfaces. The CPU waits for all outstanding instruction and data memory requests to be serviced before staring interrupt context save or IST access process.
Figure 8-55 Interrupt Processing