SLUUCF2C January 2021 – May 2022 BQ769142
| Command | Name | Access | Description |
|---|---|---|---|
| 0x000E | EXIT_DEEPSLEEP | Sealed: W Unsealed: W Full Access: W |
Exit DEEPSLEEP mode |
| 0x000F | DEEPSLEEP | Sealed: W Unsealed: W Full Access: W |
Enter DEEPSLEEP mode. Must be sent twice in a row within 4 s to take effect |
| 0x0010 | SHUTDOWN | Sealed: W Unsealed: W Full Access: W |
Start SHUTDOWN sequence. Must be sent twice in a row within 4s to take effect if sealed. If sent twice while unsealed, the shutdown delays are skipped. |
| 0x0012 | RESET | Sealed: — Unsealed: W Full Access: W |
Resets the device |
| 0x001C | PDSGTEST | Sealed: — Unsealed: W Full Access: W |
In FET Test mode, toggles the PDSG FET enable |
| 0x001D | FUSE_TOGGLE | Sealed: — Unsealed: W Full Access: W |
Toggle FUSE state |
| 0x001E | PCHGTEST | Sealed: — Unsealed: W Full Access: W |
In FET Test mode, toggles the PCHG FET enable |
| 0x001F | CHGTEST | Sealed: — Unsealed: W Full Access: W |
In FET Test mode, toggles the CHG FET enable |
| 0x0020 | DSGTEST | Sealed: — Unsealed: W Full Access: W |
In FET Test mode, toggles the DSG FET enable |
| 0x0022 | FET_ENABLE | Sealed: — Unsealed: W Full Access: W |
Toggle FET_EN
in Manufacturing Status. FET_EN = 0 means FET Test Mode. FET_EN = 1 means Firmware FET Control. |
| 0x0024 | PF_ENABLE | Sealed: — Unsealed: W Full Access: W |
Toggle PF_EN in Manufacturing Status |
| 0x0030 | SEAL | Sealed: — Unsealed: W Full Access: W |
Places the device in SEALED mode |
| 0x0082 | RESET_PASSQ | Sealed: W Unsealed: W Full Access: W |
Resets the integrated charge and timer. Charge resets to 0.5 userAh so that the integer portion is rounded. |
| 0x008A | PTO_RECOVER | Sealed: W Unsealed: W Full Access: W |
Triggers recovery from a Precharge Timeout (PTO) safety event. This also resets the timeout timer for an ongoing precharge cycle. |
| 0x0090 | SET_CFGUPDATE | Sealed: — Unsealed: W Full Access: W |
Enters CONFIG_UPDATE mode |
| 0x0092 | EXIT_CFGUPDATE | Sealed: W Unsealed: W Full Access: W |
Exits CONFIG_UPDATE mode. This also clears the Battery Status()[POR] and Battery Status()[WD] bits. |
| 0x0093 | DSG_PDSG_OFF | Sealed: W Unsealed: W Full Access: W |
Disables DSG and PDSG FET drivers. This subcommand should not be used if the DCHG pin is being used in DCHG mode. |
| 0x0094 | CHG_PCHG_OFF | Sealed: W Unsealed: W Full Access: W |
Disables CHG and PCHG FET drivers. This subcommand should not be used if the DDSG pin is being used in DDSG mode. |
| 0x0095 | ALL_FETS_OFF | Sealed: W Unsealed: W Full Access: W |
Disables CHG, DSG, PCHG, and PDSG FET drivers |
| 0x0096 | ALL_FETS_ON | Sealed: W Unsealed: W Full Access: W |
Allows all four FETs to be on if other safety conditions are met. This clears the states set by the DSG_PDSG_OFF, CHG_PCHG_OFF, and ALL_FETS_OFF commands. |
| 0x0099 | SLEEP_ENABLE | Sealed: W Unsealed: W Full Access: W |
Enable SLEEP mode. The default is loaded from data memory, after which this command can change the setting. |
| 0x009A | SLEEP_DISABLE | Sealed: W Unsealed: W Full Access: W |
Disable SLEEP mode. The default is loaded from data memory, after which this command can change the setting. |
| 0x009B | OCDL_RECOVER | Sealed: W Unsealed: W Full Access: W |
Recovers Overcurrent in Discharge Latch (OCDL) in the next execution of the safety engine (about 1 second). |
| 0x009C | SCDL_RECOVER | Sealed: W Unsealed: W Full Access: W |
Recovers Short Circuit in Discharge Latch (SCDL) in the next execution of the safety engine (about 1 second). |
| 0x009D | LOAD_DETECT_RESTART | Sealed: W Unsealed: W Full Access: W |
Restarts the timeout on the Load Detect (LD) pin current source if it has already triggered |
| 0x009E | LOAD_DETECT_ON | Sealed: W Unsealed: W Full Access: W |
Forces the Load Detect (LD) pin current source to be ON. This command has no effect when the device is configured for autonomous control of the current source (Protections:Load Detect:Active Time > 0). |
| 0x009F | LOAD_DETECT_OFF | Sealed: W Unsealed: W Full Access: W |
Force the Load Detect (LD) pin current source to be OFF. This command has no effect when the device is configured for autonomous control of the current source (Protections:Load Detect:Active Time > 0). |
| 0x2800 | CFETOFF_LO | Sealed: W Unsealed: W Full Access: W |
Drives the CFETOFF pin to a low state if it is configured as a GPO |
| 0x2801 | DFETOFF_LO | Sealed: W Unsealed: W Full Access: W |
Drives the DFETOFF pin to a low state if it is configured as a GPO |
| 0x2802 | ALERT_LO | Sealed: W Unsealed: W Full Access: W |
Drives the ALERT pin to a low state if it is configured as a GPO |
| 0x2806 | HDQ_LO | Sealed: W Unsealed: W Full Access: W |
Drives the HDQ pin to a low state if it is configured as a GPO |
| 0x2807 | DCHG_LO | Sealed: W Unsealed: W Full Access: W |
Drives the DCHG pin to a low state if it is configured as a GPO |
| 0x2808 | DDSG_LO | Sealed: W Unsealed: W Full Access: W |
Drives the DDSG pin to a low state if it is configured as a GPO |
| 0x2810 | CFETOFF_HI | Sealed: W Unsealed: W Full Access: W |
Drives the CFETOFF pin to a high state if it is configured as a GPO |
| 0x2811 | DFETOFF_HI | Sealed: W Unsealed: W Full Access: W |
Drives the DFETOFF pin to a high state if it is configured as a GPO |
| 0x2812 | ALERT_HI | Sealed: W Unsealed: W Full Access: W |
Drives the ALERT pin to a high state if it is configured as a GPO |
| 0x2816 | HDQ_HI | Sealed: W Unsealed: W Full Access: W |
Drives the HDQ pin to a high state if it is configured as a GPO. |
| 0x2817 | DCHG_HI | Sealed: W Unsealed: W Full Access: W |
Drives the DCHG pin to a high state if it is configured as a GPO |
| 0x2818 | DDSG_HI | Sealed: W Unsealed: W Full Access: W |
Drives the DDSG pin to a high state if it is configured as a GPO |
| 0x2857 | PF_FORCE_A | Sealed: W Unsealed: W Full Access: W |
First part of two-word command to force the command-based PF. Must be followed by PF_FORCE_B within 4s with no writes in between |
| 0x29A3 | PF_FORCE_B | Sealed: W Unsealed: W Full Access: W |
Second part of two-word command to force the command-based PF. Must be preceded by PF_FORCE_A within 4 s with no writes in between |
| 0x29BC | SWAP_COMM_MODE | Sealed: — Unsealed: W Full Access: W |
Changes to the communications mode previously configured by changing Settings:Configuration:Comm Type in CONFIG_UPDATE_MODE |
| 0x29E7 | SWAP_TO_I2C | Sealed: — Unsealed: W Full Access: W |
Selects I2C Fast mode (Settings:Configuration:Comm Type = 8) in data memory and immediately start using I2C |
| 0x7C35 | SWAP_TO_SPI | Sealed: — Unsealed: W Full Access: W |
Selects SPI with CRC mode (Settings:Configuration:Comm Type = 16) in data memory and immediately start using SPI |
| 0x7C40 | SWAP_TO_HDQ | Sealed: — Unsealed: W Full Access: W |
Selects HDQ using ALERT pin mode (Settings:Configuration:Comm Type = 3) in data memory and immediately start using HDQ |