SPRAD21I May 2022 – September 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
Schematic review checklist that can be used by custom board designers to review the custom board schematic covering specific peripherals have been added at the end of each section, sub section of the user's guide. The general recommendations, processor power and processor peripherals sections, sub sections described in the user's guide includes the checklist at the end. The schematic review checklist is categorized as General, Schematic Review, and Additional. Custom board designers can use the schematic review checklist to perform self-review of the custom board schematic design. Self-review minimizes possible schematics errors that can result in functional or performance related concerns and also reduced the reviewers efforts during formal reviews (internal or external). Schematic reviews minimizes the efforts required during custom board bring-up or performance testing resulting in increased board design quality and adherence to the planned timeline.
For information on available checklists and format, see the following FAQ: