SPRAD21I May 2022 – September 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
The recommendation is to follow the below listed processor family wise user's guides during custom board design (based on the processor family being used):
User's Guide Processor Family Wise (Hardware Design Considerations for Custom Board Design)
User's Guide Processor Family Wise (Schematic Design Guidelines and Schematic Review Checklist)
The next phase of the custom board design once the required schematics updates are complete (following the user's guide, referring to the SK schematic implementation, hardware design considerations user's guide and other collaterals on TI.com), is to perform a self-review following the review checklist provided at the end of each section of the schematic design guidelines. Schematic review checklist in excel format can be used alternatively to perform the review and the schematics in excel format can be used to track the completion of schematic review section wise.
Example of schematic review checklist sections for self-review:
The below FAQ lists the available collaterals and review steps that can be followed by custom board designer while performing a self-review of custom board schematics:
AM62x Processor Family:
AM62Ax and AM62D-Q1 Processor Family:
AM62Px Processor Family:
The below FAQ lists common errors observed (based on review of multiple customer schematics and reference to multiple collaterals). The recommendation is to read the list of errors and make the required updates to the custom board schematics: