TIDUA05B June 2015 – March 2025
Using the dual channel signal generator two coupled sine waves (same amplitude, same frequency, with a 90-degree phase shift among them) are generated and applied to the analog differential signals A+, A– and B+, B– using the J9 connector. Two differential probes are used to acquire the differential signals applied in input, while two single-ended probes are connected to the single-ended analog outputs A and B of the analog path, on connector J6, pin 18 and pin 20, respectively.
The amplitude of the outputs versus the inputs are measured in this way; at the same time, the phase shift between the differential inputs and the respective single ended output are measured. In this way, a Bode plot of the analog signal conditioning path could be calculated.
Figure 7-11 Transfer Function of Differential to Single-Ended Analog Signal Path — Channel A and BThe same measurements have been performed on the marker signal (R+/R–). Note that the phase of the R signal is less than the equivalent for A and B since the output has been measured at the input to the comparator. The decoupling filter here has a five times higher cut-off frequency (R = 20 Ω, C = 2.2 nF) versus the output filter for A and B (R = 100 Ω, C = 2.2 nF).
Figure 7-12 Transfer Function of Differential to Single-Ended Index Marker R