TIDUA05B June 2015 – March 2025
The input signals to all comparators are derived from the output of the single-ended to differential amplifier. The output signal is clamped to 3.3 V, as described earlier, and decoupled with a RC network (like R49, C54 in figure 19 for signal A) to avoid cross-talk to the analog single-ended signals A and B respectively.
The match the phase between the high-resolution path and this path, the RC decoupling network at the input to the comparator matches the RC filter (2×10 Ω and 2.2 nF) at the THS4531A output.
The TLV370x is configured as non-inverting comparator to detect the zero-crossing of the analog sin and cosine signals A and B as well as the index pulse R. Figure 4-7 shows the corresponding schematics for the signal A.
The switching threshold is set by the reference voltage VREF = 1.65 V (REF2033), which is also used to bias the single-ended analog signals for the differential to single-ended amplifiers. For each comparator, the reference input is taken from the REF2033 and decoupled with a 10-Ω series resistor and a 100-n capacitor.
A hysteresis is added for better noise immunity. The hysteresis (VTH+ – VTH–) of a non-inverting comparator can be calculated per Equation 7:

with VOut_High the high-level and VOut_Low the low level comparator output voltage, RF the feedback and RG the input resistor into the non-inverting comparator input.
For the configuration of this design as outlined in Figure 4-7, the hysteresis has been set to around 160 mV per Equation 8. Since R49 and R48 are magnitudes lower than R50, they can be neglected.

The upper and lower switching thresholds VTH+ and VTH– are defined per Equation 9 and Equation 10 with the reference voltage VREF = 1.65 V.


The lower threshold is a function of the supply voltage. However, the supply voltage tolerance of this design 5%, as typical with most designs. A ±5% tolerance with the 3.3-V supply voltage would affect the lower threshold by only by ±16 mV, resulting VTH– range from approximately 1.56 to 1.59-V, hence still acceptable.
Figure 4-7 Signal A Comparator With HysteresisThe 3.3-V supply of each comparator is decoupled with a 1-Ω series resistors and 100-nF capacitor to minimize cross-talk through the 3.3-V rail to other comparators. The RC low pass comprised of R49 and C54 is added to decouple the comparators switching node from the analog signal A/sin, which will be connected to an external ADC.
The hysteresis allows for a clean digital signal, which means it avoids fast switching due to noise around the zero crossing point. The hysteresis however introduces an additional propagation delay, which is depending on the analog signal amplitude VIN_PEAK-PEAK at the comparator input.

Assuming minimum input voltage of 0.3 VPP: The output of the differential- to single-ended amplifier (gain = 1.66) will have an amplitude of 0.5 VPP (0 to 100 kHz) and around 0.32 VPP at 500 kHz due to low-pass filter attenuation. The hysteresis corresponding phase delay of the digital signals A, B, and R will be around 30 degrees for a 0.32 VPP input at the comparator. At 500 kHz, this would translate into a total propagation delay of the comparator of around 170 ns + 40 ns = 210 ns.
Due to the low propagation delay of the TLV3201 with 40 ns only, the overall delay of the comparator block remains below 45 degrees up to 500 kHz.
The comparators for the signals B and R have the same settings. Also the buffering and gain stage for the index marker R is identical to the signals A and B. This is to ensure the phase of the index marker R is exactly in sync with the signal A and B up to a 500-kHz signal frequency. This ensures the zero Index Marker R will occur as specified, slightly before the rising edge of signals A and B. The index marker R defines the absolute zero position, and hence exact relation to signals A and B is required to avoid any position offset.