TIDUA05B June 2015 – March 2025
The first test is to verify the synchronization or skew between the digital output signals A, B, and R available at the TIDA-00176 host processor interface connector J6, pin 12 (ATTL), pin 14 (BTTL), and pin 16 (RTTL). This test is to verify the proper configuration of the TIDA-00176 comparator subsystem.
Figure 7-30 Measured TTL Signals A, B, and R at TIDA-00176 Comparators Output J6-12, 14, and 18The transitions on the comparator output signal R occur only when both A and B are low, as expected. This result means the sequence between A, B, and R signals depends on the rotation direction of the Sin/Cos encoder shaft. In Figure 7-30, the encoder is turned clockwise as the rising edge of B occurs after the rising edge of A.
A closer look to the skew between A, B, and R has been done at a higher speed of around 400 rpm and for the rising and falling edge of R.. The rising and falling edge of R still occurs when both signals A and B are low.
Note that the rotation direction of Figure 7-31 and Figure 7-32 is counter clockwise (CCW).
Figure 7-31 Falling Index Signal R versus A and B in CCW Direction
Figure 7-32 Rising Index Signal R versus A and B in CCW Direction