TIDUA05B June 2015 – March 2025
Figure 7-1 shows a picture of the TIDA-00176 analog signal chain tests.
Figure 7-1 Test
Setup for TIDA-00176 Analog Signal Chain Performance TestsThe high-resolution 16-bit signal path featuring fully differential amplifiers THS4531A and the dual 16-bit ADC ADS8353, as well as the differential to single-ended analog signal path have been tested. For the purpose, a dual output programmable function generator has been used. The inputs signals are applied at the connector J8 (differential inputs A, B, and R). The output waveforms have been collected at different probe points, depending on the signal path that was analyzed.