TIDUA05B June 2015 – March 2025
For the following tests, the entire high-resolution signal chain, featuring the differential amplifier THS4531A connected through an RC filter to the dual 16-bit ADC ADS8354 has been tested. A sinusoidal test signal has been injected at the encoder differential input pins and the 16-bit digital data has been analyzed.
The analysis has been done in the frequency domain to evaluate the performance on signal-to-noise ratio (SNR), total harmonic distortions (THD), signal-to-noise and distortion (SINAD), and effective number of bits (ENOB). Essentially, all these parameters are different ways of quantifying the noise and distortion performance of an ADC based on a fast-fourier transform (FFT) analysis. A brief introduction on the theory of signal-to-noise measurement with ADCs is provided at the end of this section.
For the test, two types of input signals were used:
The input signal is applied to one of the input channels A+, A– or B+, B– at a time, while the other channel while the other channel is unconnected. The purpose is to measure and highlight the ultra-low cross-talk level among the two channels A and B (or sine and cosine, respectively).
The DC input is used to ensure the best noise performance (since no noise comes from the input/source). The 1-kHz sine wave is used to measure the effective number of bits on the two parallel channels.
Both channels A and B were sampled at 32 kHz and 8192 consecutive 16-bit samples were acquired for each channel A and B. The DFT has been calculated for the collected data to measure the SNR and THD.
The results are presented in the following figures.
Figure 7-4 DFT of 16-Bit Channel A Output With 1.8-V DC at Input A
Figure 7-5 DFT of 16-Bit Channel B Output With 1.8-V DC at Input BIn the previous figures, the measured noise floor is below 120 dB, meaning this is the best performance that could be achieved. Also note that the plots are referred to the full scale input range, that is the maximum amplitude. 0 dB correspond to the maximum input possible for the ADS8354, which in this configuration would be 2 VPP.
The following figures show the DFT of the entire high-resolution channel with a sinusoidal input voltage of 0.6-VPP amplitude and 1 KHz. This equals around –6-dB input level versus the theoretical full scale range input.
The input signal was applied either to the channel A or channel B. The other channel was left open in order to measured cross-talk as well.
Figure 7-6 DFT of 16-Bit Channel A Output With 600-mVPP, 1-KHz Sine Wave Input Applied on Input A
Figure 7-7 DFT of 16-Bit Channel B Output With 600-mVPP, 1-KHz Sine Wave Input Applied on Input A
Figure 7-8 DFT of 16-Bit Channel B Output With 600-mVPP, 1-KHz Sine Wave Input Applied on Input B
Figure 7-9 DFT of 16-bit Channel A Output With 600-mVPP, 1-KHz Sine Wave Input Applied on Input BThese figures are referred to the theoretical full scale input range. Note that the first and second harmonics of the 1-kHz sinusoidal signal are due to the signal source itself, (normally a very aggressive notch filter is used to isolate the frequency of the test signal; refer also to SLAU515 for example).
Also note that the 1-kHz signal has a slight spread in frequency. This is not due to the TIDA-00176 hardware but due to a jitter in the F28069 software implementation, which triggered the SPI transfer to start the ADS8354 conversion (hold-mode) with a jitter of one CPU clock cycle equivalent to 12.5 ns.
The previous pictures also highlighted that there is basically no cross-talk between the two analog channels for sine (signal A+, A–) and cosine (B+, B–). The spectrum (DFT) is half the sampling frequency (the second half of the spectrum is a specular copy of the first half, so it is not shown in the plots). The Hann function (http://en.wikipedia.org/wiki/Hann_function) is used for windowing the data to obtain cleaner plots in the frequency domain.
THD, SNR and ENOB versus the full-scale signal can then be calculated for this design and are listed in Table 7-2.
| PARAMETER | VALUE (MEASURED) |
|---|---|
| SNR | 89.1 dB |
| SINAD | 88.5 dB |
| ENOB | 14.4 bit |
| Cross-Talk | –107 to –109 dB |