TIDUA05B June 2015 – March 2025
Follow these steps to setup the software:
The terminal program should display the start screen of TIDA-00176 as shown in Figure 6-3.
After the binary file has been loaded to the F28069M, Steps 4 through 7 are not required anymore. Simply reset the LaunchPad to restart the program. Ensure the F28069M is configured to boot from internal flash. Refer to the InstaSPIN-MOTION LaunchPad documentation.
Trouble-shooting: If no connection gets established, the VCP driver of the USB virtual Com port TI XDS100 Channel B needed to be enabled under Windows® 7 Device Manager. For more details, refer to the InstaSPIN-MOTION LaunchPad documentation.
Figure 6-3 TIDA-00176 User Interface at Startup