SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The TIMx clock (TIMCLK) can be sourced from BUSCLK, MFCLK and LFCLK by setting the TIMx.CLKSEL register. It can also be divided by a ratio by setting the TIMx.CLKDIV register and a prescaler (if present). The selected source clock is always available and the frequency depends on the power mode. For more information, see the Clock Module (CKM) section.
The TIMCLK can come from the following sources:
BUSCLK: the current bus clock is selected as the source for TIMx. The current bus clock depends on power domain.
TIMx also has a software mechanism for disabling the timer clock. Set TIMx.CCLKCTL.CLKEN to 0 to put the timer in an IDLE state.
TIMCLK Configuration
To configure the clock source, divider, and prescaler:
The frequency of TIMCLK is determined using Equation 16.