SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The comparator and external fault pin fault source input passes through a two TIMCLK synchronization stage and the fault input can be filtered through the glitch filter using the fault input filter (TIMA.FIFCTL) register.
The fault input glitch filter can be enabled by setting the TIMA.FIFCTL.FILTEN bit. The filter period is configured by setting the TIMA.FIFCTL.FP bit.
A consecutive period or majority voting format selected by the TIMA.FIFCTL.CPV bit is used to select the criteria for a CCP input signal.
Consecutive period - The fault input signal must be at the specified level for the defined number of FP timer clocks for the fault input to be processed.
Majority voting - The filter ignores one clock of opposite logic over the filter period. For example, over the number of FP samples of the fault input, up to 1 sample may be of an opposite logic value (glitch) without affecting the output.
The example shown in Figure 24-13 shows the difference between consecutive period and majority voting formats with a digital filter implemented to capture a fault input of 3 TIMCLK periods.