SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
In FULL channels, the DMA controller has two extended modes selected by the DMAEM bits as listed in DMA extended mode table. An graphical overview of the extended modes can be seen inDMA extended mode figuer. Each channel is individually configurable for the extended mode. For example, channel 0 can be configured in table mode while channel 1 is configured in fill mode.
| DMAEM | Extended Mode | Description |
|---|---|---|
| 0 | Normal mode | Operation is defined by DMATM |
1 | Gather mode | Used to read data from an address table and copy to configurable address |
2 | Fill mode | Used to fill predefined data patterns into memory |
3 | Table mode | Used to help configure a table of peripheral control registers |