SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The and HFCLK (HFXT, HFCLK_IN) high speed clock sources are not supported in the STOP and STANDBY operating modes. When a high-speed clock source ( , HFCLK) is enabled, entering either the STOP mode or STANDBY mode will cause SYSCTL to automatically disable the and/or HFCLK before entering STOP or STANDBY mode. Upon exit from STOP or STANDBY mode to RUN mode, SYSCTL will automatically re-enable the HFCLK if they were previously enabled before entering the low-power mode.
Before entering STOP or STANDBY for the first time after enabling the HFCLK, and after waking up from STOP or STANDBY mode, application software must wait to enter STOP or STANDBY mode until any previously enabled high speed clock sources have completed startup.
Application software must check the following before entering STOP or STANDBY mode:
In the event that the MCLK was configured to be sourced from HSCLK before entry to STOP or STANDBY, upon exit from STOP or STANDBY the MCLK will be sourced from SYSOSC initially and the CPU will be released to begin executing code at the SYSOSC frequency. SYSCTL will automatically restore the MCLK configuration to the previously selected high-speed clock when the high-speed clock has started and is ready for use. When MCLK switches back to the high-speed clock, SYSCTL will generate an HSCLK GOOD interrupt to alert the application that MCLK is again running from the high-speed clock.