The SYSOSC can be configured at 16MHz or 24MHz as
an alternative to the base frequency. To utilize these configurations, the trim
values need to be applied. Trimming is accomplished by manipulating the fields in
the SYSOSCTRIMUSER to achieve the target frequency. To trim the SYSOSC, the SYSOSC
clock can be brought out externally to a pin using the CLK_OUT unit so that it
can be measured.
Use the following procedure to derive the user trim values. The trimmed values can be programmed into the flash memory of the device to be recalled later. Each device must be trimmed individually for accuracy. SYSOSC can also be trimmed internally by using the frequency clock counter (FCC).
Trim
procedure using CLK_OUT with frequency correction loop (FCL) disabled (No ROSC
resistor)
- Enable the CLK_OUT unit and
select SYSOSC as the clock source, following the instructions in the CLK_OUT section
- Set the SYSOSC frequency to BASE
to start (ensure that the FREQ field in the SYSOSCCFG register is set to 0h for
BASE), and leave the FCL mode disabled
- Program an initial tuning for the
target frequency in the SYSOSCTRIMUSER register:
- Set the RESCOARSE trim
field in the SYSOSCTRIMUSER register to mid-range
- Set the RESFINE trim
field in the SYSOSCTRIMUSER register to mid-range
- Switch SYSOSC to the user-trimmed
frequency by selecting USER in the FREQ field of the SYSOSCCFG register
- Measure the SYSOSC frequency at
the CLK_OUT pin
- Switch SYSOSC back to BASE
frequency by selecting BASE in the FREQ field of the SYSOSCCFG register. Writing
to SYSOSCTRIMUSER requires SYSOSC to be operating at BASE frequency.
- Adjust the SYSOSCTRIMUSER
parameters to close on the target frequency:
- Set the target frequency
(16 or 24MHz) in the FREQ field of the SYSOSCTRIMUSER register
- Adjust trim parameters to
achieve 16 or 24 MHZ based on the selection made in step 7a
- Increasing the
CAP trim field in the SYSOSCTRIMUSER register will reduce the
SYSOSC range. For 24MHz, select CAP=0, and for 16MHz select
CAP=1
- Increasing the
RESCOARSE trim field in SYSOSCTRIMUSER will reduce the frequency
in large steps of approximately 1MHz
- Increasing the
RESFINE trim field in SYSOSCTRIMUSER will decrease the frequency
in small steps of approximately 100kHz
- Repeat steps 4 through 7 until
the desired accuracy has been achieved
- Save the resulting SYSOSCTRIMUSER
value for recall
Trim
procedure using CLK_OUT with frequency correction loop (FCL) enabled (ROSC resistor
present)
- First, complete the FCL disabled
trim procedure (defined above) to obtain starting values for the CAP, RESCOARSE,
and RESFINE trim fields in the SYSOSCTRIMUSER register
- Increase the RESCOARSE value by
02h from the value obtained in Step 1
- With CLK_OUT still enabled
(SYSOSC as the source for CLK_OUT), ensure that the FREQ field in the SYSOSCCFG
register is set to 0h for BASE, and enable the FCL mode by setting the SETUSEFCL
bit in the SYSOSCFCLCTL register
- Set the RDIV trim field in the
SYSOSCUSERTRIM register to mid-range
- Switch SYSOSC to the user-trimmed
frequency by selecting USER in the FREQ field of the SYSOSCCFG register
- Measure the SYSOSC frequency at
the CLK_OUT pin
- Switch SYSOSC back to BASE
frequency by selecting BASE in the FREQ field of the SYSOSCCFG register
- Adjust trim parameters to close
on the target frequency:
- Increasing the RDIV trim
field in the SYSOSCTRIMUSER register will increase the frequency in
small steps of approximately 50kHz
- Continue increasing or
decreasing RDIV if the frequency is in saturation (not appearing to
adjust)
- Repeat steps 5-8 until the
desired accuracy has been achieved
- Save the resulting SYSOSCTRIMUSER
value for recall
Note: SYSOSCTRIMUSER parameters only take effect when switching to the USER frequency. Once USER frequency is selected, changes to SYSOSCTRIMUSER have no effect. To refresh the USER values, first switch to BASE frequency, then update SYSOSCTRIMUSER, and then switch SYSOSC back to BASE frequency.