SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
DMA triggers are propagated to the DMA through the event manager. Most DMA triggers use fixed routes, but the DMA does provide two generic event subscriber ports which can be used to trigger DMA transfers through a generic route channel. See the device-specific data sheet for the complete list of DMA trigger assignments for a given device.
To determine if a particular peripheral on a device provides a fixed DMA trigger (DMA_TRIGx) from the peripheral directly to the DMA, review the DMA triggers table in the detailed description section of the device-specific data sheet. Certain peripherals can have more than one DMA trigger (for example, to enable a TX trigger and an RX trigger on a serial communication peripheral).
To select the specific peripheral event which triggers a static DMA route, configure the peripheral's DMA_TRIGx event management register set (IIDX, IMASK, RIS, MIS, ISET, and ICLR) which corresponds to the targeted DMA route. To determine which DMA_TRIGx register set corresponds with which DMA trigger, review the relevant chapter of this guide for the corresponding peripheral, or review Section 7.1.4.
Certain peripherals (such as the 12-bit DAC) do not implement a DMA_TRIGx register set for managing DMA triggers. In these cases, the DMA trigger configuration is done through peripheral-specific configuration registers.
The DMA contains two generic event subscriber ports (FSUB_x) which can be used to source a DMA trigger from any of the device's generic event channels. This can be used to enable special cases where a particular function on a peripheral generates a DMA trigger. For example, it can be desirable to trigger a DMA transfer from a timer.
To configure the event manager to trigger a DMA channel from a generic route, follow the steps below: