SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The DMA controller has seven addressing modes. The addressing mode for each DMA channel is independently configurable. For example, channel 0 can transfer between two fixed addresses, while channel 1 transfers between two blocks of addresses. The basic addressing modes are shown in basic address modes
The addressing modes are:
Gather data from address table to fixed address or block of addresses
Addressing modes 1-4 shown above are the basic adressing modes are simply configured with the DMASRCINCR and DMADSTINCR control bits and are available in all channel types. The DMASRCINCR bits select if the source address is incremented, decremented, or unchanged after each transfer. The DMADSTINCR bits select if the destination address is incremented, decremented, or unchanged after each transfer.
Addressing modes 5 -7 shown above are also configured with the DMASRCINCR and DMADSTINCR control bits along with the help of additional parameters such as DMAEM for leveraging the extended modes of the DMA. Refer to Section 5.2.4.1, Section 5.2.4.2 or [Gather Mode] for more details on how to properly configure and use the DMA in Fill-Mode, Table-Mode and Gather-Mode.
Transfers can be byte to byte, half-word to half-word, word to word, long-word to long-word, long-long-word to long-long-word or any combination of the five. When transferring a wider bit width source to a shorter bit width destination, only the lower bits of the destination data transfers. When transferring a shorter bith width source to a wider bit width destination, the upper bytes of the destination data is cleared when the transfer occurs. There is no packing or unpacking support by combining several source byte transfers to one single destination word or the reverse.