SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The MCLK is the main system clock and the root point of synchronization for all synchronized clocks (MCLK, CPUCLK, ULPCLK, MFCLK, and LFCLK). It is typically the highest speed clock in the system and supports operation up to 32MHz across the full temperature range of the device. The MCLK tree is the root source for the CPUCLK (in RUN mode), the PD1 high speed peripheral bus clock (in RUN and SLEEP modes), and the ULPCLK low power bus clock (in RUN, SLEEP, STOP, and STANDBY modes). In addition, the 4MHz MFCLK and 32kHz LFCLK outputs are synchronized to MCLK.
The MCLK output to PD1 peripherals is enabled in RUN and SLEEP modes, and disabled in all other power modes. While the MCLK output to PD1 is disabled in STOP and STANDBY modes, the MCLK tree is still running to source ULPCLK and to provide synchronization for MFCLK and LFCLK.
The MCLK source is selected with a glitch free clock mux and can be changed dynamically at runtime by user software. It can also be changed automatically by hardware when entering STOP and STANDBY modes or during an asynchronous fast clock request.The available sources for MCLK include:
After boot, MCLK is sourced from SYSOSC by default. The decision of which oscillator to use to source MCLK is important because MCLK sets both the CPUCLK frequency and the bus clock frequency for PD1 peripherals. As a result, the accuracy and the clock speed of the oscillator selected for MCLK must be appropriate not only for the operation of the CPU but also for the operation of the PD1 peripherals that use the bus clock as their functional clock.
The clock source and frequency selection decisions made for MCLK also affect ULPCLK in RUN and SLEEP modes. See the ULPCLK section for more information on how MCLK and ULPCLK are related in RUN and SLEEP mode.
Application software can change the MCLK source from SYSOSC to LFCLK in all modes by setting MCLKCFG.USELFCLK, giving the low peak current consumption with the CPU and PD1 peripherals operational. The following table gives the proper register bit configurations for selecting different clocks for MCLK in RUN and SLEEP modes.
| Desired Source | MCLKCFG.USELFCLK |
|---|---|
| SYSOSC | 0 |
| LFCLK | 1 |
To switch MCLK from SYSOSC to LFCLK in RUN mode:
To switch MCLK from LFCLK to SYSOSC in RUN mode:
To switch MCLK from SYSOSC to HSCLK:
To switch MCLK from HSCLK to SYSOSC:
An MCLK source divider (MDIV) is provided to enable MCLK operation in between the lowest SYSOSC frequency (4MHz) and the LFCLK frequency (32kHz). MDIV is for applications with a limited peak current but that still require a higher clock speed than 32kHz. MDIV supports dividing the 4MHz SYSOSC frequency by up to 16, enabling the additional MCLK frequency options given in Table 2-5. For example, a 500kHz MCLK frequency can be obtained by setting SYSOSC to 4MHz and setting MDIV to 7 (divide-by-8).
Table 2-5 shows the MCLK frequency which is realized with /2, /4, /8, and /16 MDIV configurations, but MDIV can be set to any integer divider between /2 and /16 (MDIV register values of 0x1 through 0xF, respectively, with 0x0 disabling the MDIV).
| MCLK Source | MDIV | MCLK Frequency |
|---|---|---|
| SYSOSC (4MHz) | 0 (Disabled) | 4MHz |
| 1 (/2) | 2MHz | |
| 3 (/4) | 1MHz | |
| 7 (/8) | 500kHz | |
| 15 (/16) | 250kHz |
To use MDIV to operate MCLK at an intermediate frequency below 4MHz, follow the steps below:
Several rules apply when using MDIV to reduce the MCLK frequency:
To disable MDIV: