SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
In TIMA only, there are internal and external fault inputs which can be used to control the generation of PWM signals. The intended use of these inputs is as a mechanism for internal or external circuitry to indicate a fault in the system. This allows the hardware to react quickly to the external fault while optionally signaling an interrupt for software correction and leaving the output signals in a safe state.
It is important to consider the following basic properties of faults in a system, such as:
Fault conditions are synchronously detected using TIMCLK or asynchronously detected. Synchronous faults have a configurable glitch filter and can generate a latched fault event. Asynchronous faults cannot be latched and do not generate a fault event, with a latency of 1-2 TIMCLK cycles to detect the fault and perform a configured action. The CCP output can be configured for either type of fault upon entry and exit conditions.
The fault handler logic diagrams are split into three parts: asynchronous faults, synchronous faults, and fault output generation.
Figure 24-34 shows the asynchronous fault handler logic connections.
Figure 24-35 shows the synchronous fault handler logic connections.
Figure 24-36 shows the fault output generation logic connections.
Key registers for configuring the fault handler are:
TIMA.CCACT_xy[0/1]: this register controls the actions of the signal generator of the capture-compare portion based on fault events.