SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
All transfer modes support a “stride” mode where the DMA source and destination can be incremented to a higher value (rather than +1) after a transfer. This is helpful for re-organizing the order of data between the source and destination.
To support incremental strides, set the DMADSTINCR and/or DMASRCINCR to STRIDE_n, where n is the number of destination and/or source increments. The real increments are based in terms of the definitions DMADSTWDTH and/or DMASRCWDTH, respectively. For example, if external ADC data is transmitted to the MCU as a six-word SPI frame, DMADSTINCR can be set to STRIDE_6 during a block transfer so that the destination address is incremented by 6 and the data is organized to make processing easier.