SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Application software can set the operating state of the TRNG by writing a new command value to the CMD field in the CTL register. While the TRNG state machine has 7 states, only 4 of the 7 states are entered by user control with CMDs (OFF, TEST_DIG, TEST_ANA, and NORM_FUNC). The other 3 states (PWRUP_ES, PWRDOWN_ES, and ERR) are entered by a hardware only when powering up or down the analog block or when an error condition occurs. The operating state change commands for the TRNG are given in Table 13-3.
| CMD | Mode | Description |
|---|---|---|
| 0x0 | PWROFF | The TRNG analog blocks are powered off, and the TRNG digital blocks are clock gated. |
| 0x1 | TEST_DIG | The TRNG digital power-on self-tests are executed and the result is reported in the TEST_RESULTS register. |
| 0x2 | TEST_ANA | The TRNG analog power-on self-tests are executed and the result is reported in the TEST_RESULTS register. |
| 0x3 | NORM_FUNC | The TRNG is put into normal operating mode, in which samples from the entropy source are collected, conditioned, decimated, and placed in the DATA_CAPTURE register. The continuous statistical health tests run in this mode. |
From a given state, only certain state changes are possible. For example, from OFF only a CMD to switch to NORM_FUNC is supported. From NORM_FUNC, CMDs to switch to TEST_DIG, TEST_ANA, and OFF are supported. From the ERR state, only a switch to OFF is supported. The state flow for the TRNG is given in Figure 13-2.
A new command can only be written to the CMD field after any previously issued commands have run to completion. If a command is written at an invalid time, it will be rejected and a command fail interrupt will be asserted.