The following steps are used to configure the secondary timer cross trigger (which is TIMAx in this example):
- Configure the secondary timer (triggered by the main timer) for the desired function for this timer, such as PWM output generation or using compare mode, to trigger other peripherals. See Section 24.2.5 for how to configure for PWM generation.
- Select which input trigger to use according to the device-specific data sheet. Using the example connection in Figure 24-38, TIMAx must be triggered by TIMGx and the cross trigger output 1 of TIMGx is connected to input trigger 0 of TIMAx. Therefore, select input trigger 0 of TIMAx by setting TIMA.TSEL.ETSEL bit to 0.
- Enable the input trigger function by setting the TIMA.TSEL.TE bit to 1.
- Set TIMAx.IFCTL_01[0].ISEL = 3 and TIMAx.IFCTL_01[1].ISEL = 3 to select the trigger as the input source.
- For a center-aligned PWM, set the TIMA.CCCTL_01[0].ZCOND and TIMA.CCCTL_01[1].ZCOND bits to 1 to use a trigger assertion edge for a zero event.
- For an edge-aligned PWM, set the TIMA.CCCTL_01[0].LCOND and TIMA.CCCTL_01[1].LCOND bits to 1 to use the trigger assertion edge for a load event.
- The TIMx.CTRCTL.EN bit is set as the result of an LCOND or ZCOND condition being met, and the counter value changes to the load value or zero value, respectively.
As the main timer TIMGx must also trigger itself, complete the previous configuration steps for TIMAx to trigger TIMGx itself.
Figure 24-40 shows the logic connection.
Note: Refer to "TIMx Cross Trigger Map" in the device-specific data sheet for enabled cross trigger mapping using the ETSEL bit. For instance, if the timer instances of a device all use trigger input 0 (TRIG0) to cross trigger other timers, then only TRIG0 can be used to cross trigger other instances.