SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The power management and clock unit (PMCU) provides all power, clocking, reset, and system control services for the device. The PMCU contains three submodules to provide this functionality: the power management unit (PMU), the clock module (CKM), and the system controller (SYSCTL).
The PMU is an analog submodule that generates the internal regulated supplies for the device and supervises the condition of the external supply. The PMU also contains voltage and current reference circuits used by the on-chip regulators and analog peripherals.
The CKM is an analog submodule that provides clock sources (internal oscillators) and presents these clock sources to SYSCTL. SYSCTL distributes these clock sources to the CPU, buses, and peripherals on the device.
The SYSCTL is a digital submodule that provides the control logic for all functions in the PMCU. In addition, SYSCTL contains the memory-mapped registers used by software to configure power management and clocks, assess the status of the device, and control resets. SYSCTL also provides general-purpose memory that is retained in SHUTDOWN mode and can be used to store status information in SHUTDOWN mode when SRAM and register contents are lost.
Figure 2-1 shows the interfaces between the PMCU and the device supplies, clocks, and signals. Configuration of the PMCU by software is always done through memory-mapped registers in the SYSCTL submodule.
Using this Guide
The PMU, CKM, and SYSCTL sections of this chapter describe the functionality provided by each submodule in detail.
The quick start section describes overall system level operation of the PMCU and how to configure the PMCU for different application scenarios.