SWCU195A December 2024 ā May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Most crypto acceleration on the CC27XX device requires the HSM FW to function. See Chapter 8 for more details. By default, the SimpleLink⢠Low Power F3 Software Development Kit (SDK) will provide HSM FW, which has been encrypted and signed by Texas Instruments.
If it is desired to additionally require HSM FW to be signed by a customer private key, do the following below. See the SDK Quick Start Guide as well as the `hsmFwUpdate` example in the SDK for more details. Using those guides, scripts, and examples, you will be walked through how to:
Create an RSA 3K private/public key pair.
Obtain the correct public key digest/hash and configure the SCFG accordingly.
Sign the default HSM FW image from the SDK with your private key.
When this is done, only HSM FW, which has been signed by your company's private key, will be accepted by the device.