SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
This channel action continuously does the following:
The channel generates an edge-aligned PWM waveform when CTL.MODE = UP_PER. The channel copies a new value written in PCnCC to CnCC when CNTR becomes 0. This prevents jitter on the edges of the generated PWM signal. Similarly, the timer copies a new value written in PTGT to TGT when CNTR becomes 0. This avoids period-jitter in PWM applications with time-varying period.
Example: Edge-Aligned PWM Generation by Channel 0
This example illustrates edge-aligned PWM generation by channel 0 (see below). The waveform is synthesized on event output 0. The timer period is kept static, and the target value is set to period minus 1. Configure as follows:
The duty-cycle of the generated PWM waveform is controlled by PC0CC updates. Waveform generation on event output 0 continues until aborted by the user.