SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
The ROM API is the mechanism in which an Application (or an SSB) communicates with System ROM to request commands to Secure Boot. Similarly, Secure Boot will use the ROM API to communicate to the Application (or SSB) the status of the operation that was requested.
In general, the target being executed needs to set the ID and Sector (using the HAPI described below), and then issue a device reset. ROM Secure Boot will then take control and perform the requested actions.