SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
The filter matches for all received frames with Message IDs in the range defined by SF1ID/SF2ID resp. EF1ID/EF2ID.
There are two possibilities when range filtering is used together with extended frames:
EFT = “00”: The Message ID of received frames is ANDed with the Extended ID AND Mask (XIDAM) before the range filter is applied
EFT = “11”: The Extended ID AND Mask (XIDAM) is not used for range filtering