SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
The device has a single voltage domain, VDDD. Within VDDD, there are two power domains. The always-on AON domain and the switchable MCU domain. Throughout this documentation, register mnemonics or descriptions can also reference the ULL domain, which is an alternative term for AON and is equivalent in all ways. Similarly, the MCU domain can be described in register mnemonics or descriptions as SVT. See Figure 6-2 and Figure 6-3 for an overview of the voltage and power partitioning.