SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
Table 12-94 lists the memory-mapped registers for the LGPT2 registers. All register offset addresses not listed in Table 12-94 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Section |
|---|---|---|---|
| 0h | DESC | Description Register. | Section 12.7.1 |
| 4h | DESCEX | Description Extended | Section 12.7.2 |
| 8h | STARTCFG | Start Configuration | Section 12.7.3 |
| Ch | CTL | Timer Control | Section 12.7.4 |
| 10h | OUTCTL | Output Control | Section 12.7.5 |
| 14h | CNTR | Counter | Section 12.7.6 |
| 18h | PRECFG | Clock Prescaler Configuration | Section 12.7.7 |
| 1Ch | PREEVENT | Prescaler Event | Section 12.7.8 |
| 20h | CHFILT | Channel Input Filter | Section 12.7.9 |
| 34h | QDECSTAT | Quadrature Decoder Status | Section 12.7.10 |
| 3Ch | DMA | Direct Memory Accsess | Section 12.7.11 |
| 40h | DMARW | Direct Memory Access | Section 12.7.12 |
| 44h | ADCTRG | ADC Trigger | Section 12.7.13 |
| 48h | IOCTL | IO Controller | Section 12.7.14 |
| 68h | IMASK | Interrupt mask. | Section 12.7.15 |
| 6Ch | RIS | Raw interrupt status. | Section 12.7.16 |
| 70h | MIS | Masked interrupt status. | Section 12.7.17 |
| 74h | ISET | Interrupt set register. | Section 12.7.18 |
| 78h | ICLR | Interrupt clear register. | Section 12.7.19 |
| 7Ch | IMSET | Interrupt mask set register. | Section 12.7.20 |
| 80h | IMCLR | Interrupt mask clear register. | Section 12.7.21 |
| 84h | EMU | Debug control | Section 12.7.22 |
| C0h | C0CFG | Channel 0 Configuration | Section 12.7.23 |
| C4h | C1CFG | Channel 1 Configuration | Section 12.7.24 |
| C8h | C2CFG | Channel 2 Configuration | Section 12.7.25 |
| FCh | PTGT | Pipeline Target | Section 12.7.26 |
| 100h | PC0CC | Pipeline Channel 0 Capture Compare | Section 12.7.27 |
| 104h | PC1CC | Pipeline Channel 1 Capture Compare | Section 12.7.28 |
| 108h | PC2CC | Pipeline Channel 2 Capture Compare | Section 12.7.29 |
| 13Ch | TGT | Target | Section 12.7.30 |
| 140h | C0CC | Channel 0 Capture Compare | Section 12.7.31 |
| 144h | C1CC | Channel 1 Capture Compare | Section 12.7.32 |
| 148h | C2CC | Channel 2 Capture Compare | Section 12.7.33 |
| 17Ch | PTGTNC | Pipeline Target No Clear | Section 12.7.34 |
| 180h | PC0CCNC | Pipeline Channel 0 Capture Compare No Clear | Section 12.7.35 |
| 184h | PC1CCNC | Pipeline Channel 1 Capture Compare No Clear | Section 12.7.36 |
| 188h | PC2CCNC | Pipeline Channel 2 Capture Compare No Clear | Section 12.7.37 |
| 1BCh | TGTNC | Target No Clear | Section 12.7.38 |
| 1C0h | C0CCNC | Channel 0 Capture Compare No Clear | Section 12.7.39 |
| 1C4h | C1CCNC | Channel 1 Capture Compare No Clear | Section 12.7.40 |
| 1C8h | C2CCNC | Channel 2 Capture Compare No Clear | Section 12.7.41 |
Complex bit access types are encoded to fit into small table cells. Table 12-95 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
DESC is shown in Table 12-96.
Return to the Summary Table.
Description Register.
This register provides IP module ID, revision information, instance index and standard MMR registers offset.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | MODID | R | DE49h | Module identifier used to uniquely identify this IP. |
| 15-12 | STDIPOFF | R | 1h | Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB. 0: Standard IP MMRs do not exist 0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address) |
| 11-8 | INSTIDX | R | 0h | IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number. |
| 7-4 | MAJREV | R | 1h | Major revision of IP. |
| 3-0 | MINREV | R | 1h | Minor revision of IP. |
DESCEX is shown in Table 12-97.
Return to the Summary Table.
Description Extended
This register describes the parameters of the LGPT.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-20 | RESERVED | R | 0h | Reserved |
| 19 | HIR | R | 0h | Has IR logic. |
| 18 | HDBF | R | 0h | Has Dead-Band, Fault, and Park logic. |
| 17-14 | PREW | R | 8h | Prescale width. The prescaler can maximum be configured to 2PREW-1. |
| 13 | HQDEC | R | 1h | Has Quadrature Decoder. |
| 12 | HCIF | R | 1h | Has channel input filter. |
| 11-8 | CIFS | R | 8h | Channel input filter size. The prevailing state filter can maximum be configured to 2CIFS-1. |
| 7 | HDMA | R | 1h | Has uDMA output and logic. |
| 6 | HINT | R | 1h | Has interrupt output and logic. |
| 5-4 | CNTRW | R | 0h | Counter bit-width. The maximum counter value is equal to 2CNTRW-1.
|
| 3-0 | NCH | R | 3h | Number of channels. |
STARTCFG is shown in Table 12-98.
Return to the Summary Table.
Start Configuration
This register is only for when CTL.MODE is configured to one of the SYNC modes.
This register defines when this LGPT starts.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1-0 | LGPT0 | R/W | 0h | LGPT start |
CTL is shown in Table 12-99.
Return to the Summary Table.
Timer Control
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2RST | W | 0h | Channel 2 reset.
|
| 9 | C1RST | W | 0h | Channel 1 reset.
|
| 8 | C0RST | W | 0h | Channel 0 reset.
|
| 7-6 | RESERVED | R | 0h | Reserved |
| 5 | INTP | R/W | 0h | Interrupt Phase. This bit field controls when the RIS.TGT and RIS.ZERO interrupts are set.
|
| 4-3 | CMPDIR | R/W | 0h | Compare direction. This bit field controls the direction the counter must have in order to set the RIS.CnCC channel interrupts. This bitfield is only relevant if [CnCFG.CCACT] is configured to a compare action.
|
| 2-0 | MODE | R/W | 0h | Timer mode control The CNTR restarts from 0 when MODE is written to UP_ONCE, UP_PER, UPDWN_PER, QDEC, SYNC_UP_ONCE, SYNC_UP_PER or SYNC_UPDWN_PER. When writing MODE all internally queued updates to the channels and TGT is cleared. When configuring the timer, MODE should be the last thing to configure. If changing timer configuration after MODE has been set is necessary, instructions, if any, given in the configuration registers should be followed. See for example C0CFG.
|
OUTCTL is shown in Table 12-100.
Return to the Summary Table.
Output Control
Set and clear individual outputs manually. Manual update of an output takes priority over automatic channel updates to the same output. It is not possible to set and clear an output at the same time, such requests will be neglected.
An output can be automatically cleared, set, toggled, or pulsed by each channel, listed in decreasing order of priority. The action with highest priority happens when multiple channels want to update an output at the same time.
All outputs are connected to the event fabric and the IO controller. The outputs going to the IO controller have an aditional complementary output, this output is the inverted IO output. Both the IO and the IO complementary outputs are passed through an IO Controller, see IOCTL.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-6 | RESERVED | R | 0h | Reserved |
| 5 | SETOUT2 | W | 0h | Set output 2. Write 1 to set output 2. |
| 4 | CLROUT2 | W | 0h | Clear output 2. Write 1 to clear output 2. |
| 3 | SETOUT1 | W | 0h | Set output 1. Write 1 to set output 1. |
| 2 | CLROUT1 | W | 0h | Clear output 1. Write 1 to clear output 1. |
| 1 | SETOUT0 | W | 0h | Set output 0. Write 1 to set output 0. |
| 0 | CLROUT0 | W | 0h | Clear output 0. Write 1 to clear output 0. |
CNTR is shown in Table 12-101.
Return to the Summary Table.
Counter
The counter of this timer. After CTL.MODE is set the counter updates at the rate specified in PRECFG.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Current counter value. If CTL.MODE = QDEC this can be used to set the initial counter value during QDEC. Writing to CNTR in other modes than QDEC is possible, but may result in unpredictable behavior. |
PRECFG is shown in Table 12-102.
Return to the Summary Table.
Clock Prescaler Configuration
This register is used to set the timer clock period. The prescaler is a counter which counts down from the value TICKDIV. When the prescaler counter reaches zero, CNTR is updated. The field TICKDIV effectively divides the prescaler tick source. The timer clock frequency can be calculated as TICKSRC/(TICKDIV+1).
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | TICKDIV | R/W | 0h | Tick division. TICKDIV determines the timer clock frequency for the counter, and timer output updates. The timer clock frequency is the clock selected by TICKSRC divided by (TICKDIV + 1). This inverse is the timer clock period. 0x00: Divide by 1. 0x01: Divide by 2. ... 0xFF: Divide by 256. |
| 7-2 | RESERVED | R | 0h | Reserved |
| 1-0 | TICKSRC | R/W | 0h | Prescaler tick source. TICKSRC determines the source which decrements the prescaler.
|
PREEVENT is shown in Table 12-103.
Return to the Summary Table.
Prescaler Event
This register is used to output a logic high signal before the zero crossing of the prescaler counter. The output is routed to the IOC.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7-0 | VAL | R/W | 0h | Sets the HIGH time of the prescaler event output. Event goes high when the prescaler counter equals VAL. Event goes low when prescaler counter is 0. Note: - Can be used to precharge or turn an external component on for a short time before sampling, like in QDEC. - If there is a requirement to create such events that have very short periods compared to timer clock period, use two timers. One timer acts as prescaler and event generator for another timer. |
CHFILT is shown in Table 12-104.
Return to the Summary Table.
Channel Input Filter
This register is used to configure the filter on the channel inputs. The configuration is for all inputs.
The filter is enabled when a channel is in capture mode.
The input to the filter is passed to the edge detection logic if LOAD + 1 consecutive input samples are equal. The filter functions as a down counter, counting down every input sample.
If two consecutive samples are unequal, the filter counter restarts from LOAD.
If the filter counter reaches zero, the input signal is valid and passed to the edge detection logic.
The channel filter should only be configured while the CTL.MODE = DIS. Configuring the filter while the timer is running can result in unexpected behavior.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | LOAD | R/W | 0h | The input of the channel filter is passed to the edge detection logic after LOAD + 1 consecutive equal samples. |
| 7-2 | RESERVED | R | 0h | Reserved |
| 1-0 | MODE | R/W | 0h | Channel filter mode
|
QDECSTAT is shown in Table 12-105.
Return to the Summary Table.
Quadrature Decoder Status
This register can be used during QDEC mode to check the status of the quadrature decoder.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | DBLTRANS | R | 0h | Double transition
|
| 0 | QDIR | R | 0h | Direction of count during QDEC mode.
|
DMA is shown in Table 12-106.
Return to the Summary Table.
Direct Memory Accsess
This register is used to enable DMA requests from the timer and set the register addresses which the DMA will access (read/write).
Choose DMA request source by setting the REQ field. The setting of the corresponding interrupt in the RIS registers also sets the DMA request.
Upon a DMA request defined by REQ an internal address pointer is set to RWADDR*4. Every access to DMARW will increment the internal pointer by 4 such that the next DMA access will be to the next register.
The internal pointer will stop after RWCNTR increments. Further access will be ignored.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-20 | RESERVED | R | 0h | Reserved |
| 19-16 | RWCNTR | R/W | 0h | The read/write counter. RWCNTR+1 is the number of times the DMA can access (read/write) the DMARW register. For each DMA access to DMARW an internal counter is incremented, writing to the next address field. RWADDR + 4*RWCNTR is the final register address which can be accessed by the DMA. |
| 15 | RESERVED | R | 0h | Reserved |
| 14-8 | RWADDR | R/W | 0h | The base address which the DMA access when reading/writing DMARW. The base address is set by taking the 9 LSB of the physical address and divide by 4. For example, if you wanted the RWADDR to point to the PTGT register you should set RWADDR = 0x0FC/4. |
| 7-4 | RESERVED | R | 0h | Reserved |
| 3-0 | REQ | R/W | 0h |
|
DMARW is shown in Table 12-107.
Return to the Summary Table.
Direct Memory Access
This register is used by the DMA to access (read/write) register inside this LGPT module.
Each access to this register will increment the internal DMA address counter. See DMA for description.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | DMA read write value. The value that is read/written from/to the registers. |
ADCTRG is shown in Table 12-108.
Return to the Summary Table.
ADC Trigger
This register is used to enable ADC trigger from the timer.
Choose ADC trigger source by setting the SRC field. The setting of the corresponding interrupt in the RIS registers also sets the ADC trigger.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | SRC | R/W | 0h |
|
IOCTL is shown in Table 12-109.
Return to the Summary Table.
IO Controller
This register overrides the IO outputs.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-12 | RESERVED | R | 0h | Reserved |
| 11-10 | COUT2 | R/W | 0h | IO complementary output 2 control This bit field controls IO complementary output 2.
|
| 9-8 | OUT2 | R/W | 0h | IO output 2 control This bit field controls IO output 2.
|
| 7-6 | COUT1 | R/W | 0h | IO complementary output 1 control This bit field controls IO complementary output 1.
|
| 5-4 | OUT1 | R/W | 0h | IO output 1 control This bit field controls IO output 1.
|
| 3-2 | COUT0 | R/W | 0h | IO complementary output 0 control This bit field controls IO complementary output 0.
|
| 1-0 | OUT0 | R/W | 0h | IO output 0 control This bit field controls IO output 0.
|
IMASK is shown in Table 12-110.
Return to the Summary Table.
Interrupt mask.
This register selects interrupt sources which are allowed to pass from RIS to MIS when the corresponding bit-fields are set to 1.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | R/W | 0h | Enable RIS.C2CC interrupt.
|
| 9 | C1CC | R/W | 0h | Enable RIS.C1CC interrupt.
|
| 8 | C0CC | R/W | 0h | Enable RIS.C0CC interrupt.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | R/W | 0h | Enable RIS.FAULT interrupt.
|
| 5 | IDX | R/W | 0h | Enable RIS.IDX interrupt.
|
| 4 | DIRCHNG | R/W | 0h | Enable RIS.DIRCHNG interrupt.
|
| 3 | CNTRCHNG | R/W | 0h | Enable RIS.CNTRCHNG interrupt.
|
| 2 | DBLTRANS | R/W | 0h | Enable RIS.DBLTRANS interrupt.
|
| 1 | ZERO | R/W | 0h | Enable RIS.ZERO interrupt.
|
| 0 | TGT | R/W | 0h | Enable RIS.TGT interrupt.
|
RIS is shown in Table 12-111.
Return to the Summary Table.
Raw interrupt status.
This register reflects the state of all pending interrupts, regardless of masking. This register allows the user to implement a poll scheme. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | R | 0h | Status of the C2CC interrupt. The interrupt is set when C2CC has capture or compare event.
|
| 9 | C1CC | R | 0h | Status of the C1CC interrupt. The interrupt is set when C1CC has capture or compare event.
|
| 8 | C0CC | R | 0h | Status of the C0CC interrupt. The interrupt is set when C0CC has capture or compare event.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | R | 0h | Status of the FAULT interrupt. The interrupt is set immediately on active fault input.
|
| 5 | IDX | R | 0h | Status of the IDX interrupt. The interrupt is set when IDX is active.
|
| 4 | DIRCHNG | R | 0h | Status of the DIRCHNG interrupt. The interrupt is set when the direction of the counter changes.
|
| 3 | CNTRCHNG | R | 0h | Status of the CNTRCHNG interrupt. The interrupt is set when the counter increments or decrements.
|
| 2 | DBLTRANS | R | 0h | Status of the DBLTRANS interrupt. The interrupt is set when a double transition has happened during QDEC mode.
|
| 1 | ZERO | R | 0h | Status of the ZERO interrupt. The interrupt is set when CNTR = 0.
|
| 0 | TGT | R | 0h | Status of the TGT interrupt. The interrupt is set when CNTR = TGT.
|
MIS is shown in Table 12-112.
Return to the Summary Table.
Masked interrupt status.
This register is simply a bitwise AND of the contents of IMASK and RIS.*] registers. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | R | 0h | Masked status of the RIS.C2CC interrupt.
|
| 9 | C1CC | R | 0h | Masked status of the RIS.C1CC interrupt.
|
| 8 | C0CC | R | 0h | Masked status of the RIS.C0CC interrupt.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | R | 0h | Masked status of the RIS.FAULT interrupt.
|
| 5 | IDX | R | 0h | Masked status of the RIS.IDX interrupt.
|
| 4 | DIRCHNG | R | 0h | Masked status of the RIS.DIRCHNG interrupt.
|
| 3 | CNTRCHNG | R | 0h | Masked status of the RIS.CNTRCHNG interrupt.
|
| 2 | DBLTRANS | R | 0h | Masked status of the RIS.DBLTRANS interrupt.
|
| 1 | ZERO | R | 0h | Masked status of the RIS.ZERO interrupt.
|
| 0 | TGT | R | 0h | Masked status of the RIS.TGT interrupt.
|
ISET is shown in Table 12-113.
Return to the Summary Table.
Interrupt set register.
This register can used by software for diagnostics and safety checking purposes. Writing a 1 to a bit in this register will set the event and the corresponding RIS bit also gets set. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets set.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | W | 0h | Set the RIS.C2CC interrupt.
|
| 9 | C1CC | W | 0h | Set the RIS.C1CC interrupt.
|
| 8 | C0CC | W | 0h | Set the RIS.C0CC interrupt.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | W | 0h | Set the RIS.FAULT interrupt.
|
| 5 | IDX | W | 0h | Set the RIS.IDX interrupt.
|
| 4 | DIRCHNG | W | 0h | Set the RIS.DIRCHNG interrupt.
|
| 3 | CNTRCHNG | W | 0h | Set the RIS.CNTRCHNG interrupt.
|
| 2 | DBLTRANS | W | 0h | Set the RIS.DBLTRANS interrupt.
|
| 1 | ZERO | W | 0h | Set the RIS.ZERO interrupt.
|
| 0 | TGT | W | 0h | Set the RIS.TGT interrupt.
|
ICLR is shown in Table 12-114.
Return to the Summary Table.
Interrupt clear register.
This register allows software to clear interrupts. Writing a 1 to a bit in this register will clear the event and the corresponding RIS bit also gets cleared. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets cleared.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | W | 0h | Clear the RIS.C2CC interrupt.
|
| 9 | C1CC | W | 0h | Clear the RIS.C1CC interrupt.
|
| 8 | C0CC | W | 0h | Clear the RIS.C0CC interrupt.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | W | 0h | Clear the RIS.FAULT interrupt.
|
| 5 | IDX | W | 0h | Clear the RIS.IDX interrupt.
|
| 4 | DIRCHNG | W | 0h | Clear the RIS.DIRCHNG interrupt.
|
| 3 | CNTRCHNG | W | 0h | Clear the RIS.CNTRCHNG interrupt.
|
| 2 | DBLTRANS | W | 0h | Clear the RIS.DBLTRANS interrupt.
|
| 1 | ZERO | W | 0h | Clear the RIS.ZERO interrupt.
|
| 0 | TGT | W | 0h | Clear the RIS.TGT interrupt.
|
IMSET is shown in Table 12-115.
Return to the Summary Table.
Interrupt mask set register.
Writing a 1 to a bit in this register will set the corresponding IMASK bit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | W | 0h | Set the MIS.C2CC mask.
|
| 9 | C1CC | W | 0h | Set the MIS.C1CC mask.
|
| 8 | C0CC | W | 0h | Set the MIS.C0CC mask.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | W | 0h | Set the MIS.FAULT mask.
|
| 5 | IDX | W | 0h | Set the MIS.IDX mask.
|
| 4 | DIRCHNG | W | 0h | Set the MIS.DIRCHNG mask.
|
| 3 | CNTRCHNG | W | 0h | Set the MIS.CNTRCHNG mask.
|
| 2 | DBLTRANS | W | 0h | Set the MIS.DBLTRANS mask.
|
| 1 | ZERO | W | 0h | Set the MIS.ZERO mask.
|
| 0 | TGT | W | 0h | Set the MIS.TGT mask.
|
IMCLR is shown in Table 12-116.
Return to the Summary Table.
Interrupt mask clear register.
Writing a 1 to a bit in this register will clear the corresponding IMASK bit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | C2CC | W | 0h | Clear the MIS.C2CC mask.
|
| 9 | C1CC | W | 0h | Clear the MIS.C1CC mask.
|
| 8 | C0CC | W | 0h | Clear the MIS.C0CC mask.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | FAULT | W | 0h | Clear the MIS.FAULT mask.
|
| 5 | IDX | W | 0h | Clear the MIS.IDX mask.
|
| 4 | DIRCHNG | W | 0h | Clear the MIS.DIRCHNG mask.
|
| 3 | CNTRCHNG | W | 0h | Clear the MIS.CNTRCHNG mask.
|
| 2 | DBLTRANS | W | 0h | Clear the MIS.DBLTRANS mask.
|
| 1 | ZERO | W | 0h | Clear the MIS.ZERO mask.
|
| 0 | TGT | W | 0h | Clear the MIS.TGT mask.
|
EMU is shown in Table 12-117.
Return to the Summary Table.
Debug control
This register can be used to freeze the timer when CPU halts when HALT is set to 1. When HALT is set to 0, or when the CPU releases debug halt, the filters and edge detection logic is flushed and the timer starts. For setting a predefined output value during a CPU debug halt, PARK, if the timer has this register, should be configured additionally. If this timer does not have the PARK register a predefined output value during CPU halt is not possible.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | CTL | R/W | 0h | Halt control. Configure when the counter shall stop upon CPU halt. This bitfield only applies if HALT = 1.
|
| 0 | HALT | R/W | 0h | Halt LGPT when CPU is halted in debug.
|
C0CFG is shown in Table 12-118.
Return to the Summary Table.
Channel 0 Configuration
This register configures channel function and enables outputs.
Each channel has an edge-detection circuit. The the edge-detection circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and CTL.MODE is changed from DIS to another mode.
The flush action uses two system clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
The channel input signal enters the edge-detection circuit. False capture events can occur when:
- the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described above.
- the CCACT field is reconfigured while CTL.MODE is different from DIS.
Primary use scenario is to select CCACT before starting the timer. Follow these steps to configure CCACT to a capture action while CTL.MODE is different from DIS:
- Set EDGE to NONE.
- Configure CCACT.
- Wait for three system clock periods before setting EDGE different from NONE.
These steps prevent capture events caused by expired signal values in edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | OUT2 | R/W | 0h | Output 2 enable. When 0 < CCACT < 8, OUT2 becomes zero after a capture or compare event.
|
| 9 | OUT1 | R/W | 0h | Output 1 enable. When 0 < CCACT < 8, OUT1 becomes zero after a capture or compare event.
|
| 8 | OUT0 | R/W | 0h | Output 0 enable. When 0 < CCACT < 8, OUT0 becomes zero after a capture or compare event.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | INPUT | R/W | 0h | Select channel input.
|
| 5-4 | EDGE | R/W | 0h | Determines the edge that triggers the channel input event. This happens post filter.
|
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. In every compare event the timer looks at the current value of CNTR. The corresponding output event will be set 1 timer period after CNTR = C0CC.
|
C1CFG is shown in Table 12-119.
Return to the Summary Table.
Channel 1 Configuration
This register configures channel function and enables outputs.
Each channel has an edge-detection circuit. The the edge-detection circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and CTL.MODE is changed from DIS to another mode.
The flush action uses two system clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
The channel input signal enters the edge-detection circuit. False capture events can occur when:
- the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described above.
- the CCACT field is reconfigured while CTL.MODE is different from DIS.
Primary use scenario is to select CCACT before starting the timer. Follow these steps to configure CCACT to a capture action while CTL.MODE is different from DIS:
- Set EDGE to NONE.
- Configure CCACT.
- Wait for three system clock periods before setting EDGE different from NONE.
These steps prevent capture events caused by expired signal values in edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | OUT2 | R/W | 0h | Output 2 enable. When 0 < CCACT < 8, OUT2 becomes zero after a capture or compare event.
|
| 9 | OUT1 | R/W | 0h | Output 1 enable. When 0 < CCACT < 8, OUT1 becomes zero after a capture or compare event.
|
| 8 | OUT0 | R/W | 0h | Output 0 enable. When 0 < CCACT < 8, OUT0 becomes zero after a capture or compare event.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | INPUT | R/W | 0h | Select channel input.
|
| 5-4 | EDGE | R/W | 0h | Determines the edge that triggers the channel input event. This happens post filter.
|
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. In every compare event the timer looks at the current value of CNTR. The corresponding output event will be set 1 timer period after CNTR = C1CC.
|
C2CFG is shown in Table 12-120.
Return to the Summary Table.
Channel 2 Configuration
This register configures channel function and enables outputs.
Each channel has an edge-detection circuit. The the edge-detection circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and CTL.MODE is changed from DIS to another mode.
The flush action uses two system clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
The channel input signal enters the edge-detection circuit. False capture events can occur when:
- the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described above.
- the CCACT field is reconfigured while CTL.MODE is different from DIS.
Primary use scenario is to select CCACT before starting the timer. Follow these steps to configure CCACT to a capture action while CTL.MODE is different from DIS:
- Set EDGE to NONE.
- Configure CCACT.
- Wait for three system clock periods before setting EDGE different from NONE.
These steps prevent capture events caused by expired signal values in edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10 | OUT2 | R/W | 0h | Output 2 enable. When 0 < CCACT < 8, OUT2 becomes zero after a capture or compare event.
|
| 9 | OUT1 | R/W | 0h | Output 1 enable. When 0 < CCACT < 8, OUT1 becomes zero after a capture or compare event.
|
| 8 | OUT0 | R/W | 0h | Output 0 enable. When 0 < CCACT < 8, OUT0 becomes zero after a capture or compare event.
|
| 7 | RESERVED | R | 0h | Reserved |
| 6 | INPUT | R/W | 0h | Select channel input.
|
| 5-4 | EDGE | R/W | 0h | Determines the edge that triggers the channel input event. This happens post filter.
|
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. In every compare event the timer looks at the current value of CNTR. The corresponding output event will be set 1 timer period after CNTR = C2CC.
|
PTGT is shown in Table 12-121.
Return to the Summary Table.
Pipeline Target
A read or write to this register will clear the RIS.ZERO and RIS.TGT interrupt.
If CTL.MODE != QDEC.
Target value for next counter period.
The timer will copy PTGT.VAL to TGT.VAL on the upcoming CNTR zero crossing only if PTGT.VAL has been written. The copy does not happen when restarting the timer.
This is useful to avoid period jitter in PWM applications with time-varying period, sometimes referenced as phase corrected PWM.
If CTL.MODE = QDEC
The CNTR value is updated with VALUE on IDX if the counter is counting down. If the counter is counting up, CNTR is loaded with zero on IDX.
In this mode the VALUE is not loaded into TGT on zero crossing.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | The pipleline target value. |
PC0CC is shown in Table 12-122.
Return to the Summary Table.
Pipeline Channel 0 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will clear the RIS.C0CC interrupt. Compare mode: An update of VAL will be transferred to C0CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C0CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C0CFG.EDGE. |
PC1CC is shown in Table 12-123.
Return to the Summary Table.
Pipeline Channel 1 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will clear the RIS.C1CC interrupt. Compare mode: An update of VAL will be transferred to C1CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C1CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C1CFG.EDGE. |
PC2CC is shown in Table 12-124.
Return to the Summary Table.
Pipeline Channel 2 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will clear the RIS.C2CC interrupt. Compare mode: An update of VAL will be transferred to C2CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C2CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C2CFG.EDGE. |
TGT is shown in Table 12-125.
Return to the Summary Table.
Target
User defined counter target.
A read or write to this register will clear the RIS.ZERO and RIS.TGT interrupt.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | FFFFh | User defined counter target value. |
C0CC is shown in Table 12-126.
Return to the Summary Table.
Channel 0 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will clear the RIS.C0CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C0CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C0CFG.CCACT determines if VAL is a signal period or a regular capture value. |
C1CC is shown in Table 12-127.
Return to the Summary Table.
Channel 1 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will clear the RIS.C1CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C1CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C1CFG.CCACT determines if VAL is a signal period or a regular capture value. |
C2CC is shown in Table 12-128.
Return to the Summary Table.
Channel 2 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will clear the RIS.C2CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C2CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C2CFG.CCACT determines if VAL is a signal period or a regular capture value. |
PTGTNC is shown in Table 12-129.
Return to the Summary Table.
Pipeline Target No Clear
Use this register to read or write to PTGT without clearing the RIS.ZERO and RIS.TGT interrupt.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | A read or write to this register will not clear the RIS.TGT interrupt. If CTL.MODE != QDEC. Target value for next counter period. The timer copies VAL to TGT.VAL when CNTR.VAL becomes 0. The copy does not happen when restarting the timer. This is useful to avoid period jitter in PWM applications with time-varying period, sometimes referenced as phase corrected PWM. If CTL.MODE = QDEC. The CNTR.VAL is updated with VAL on IDX. VAL is not loaded into TGT.VAL when CNTR.VAL becomes 0. |
PC0CCNC is shown in Table 12-130.
Return to the Summary Table.
Pipeline Channel 0 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C0CC interrupt. Compare mode: An update of VAL will be transferred to C0CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C0CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C0CFG.EDGE. |
PC1CCNC is shown in Table 12-131.
Return to the Summary Table.
Pipeline Channel 1 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C1CC interrupt. Compare mode: An update of VAL will be transferred to C1CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C1CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C1CFG.EDGE. |
PC2CCNC is shown in Table 12-132.
Return to the Summary Table.
Pipeline Channel 2 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Pipeline Capture Compare value. User defined pipeline compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C2CC interrupt. Compare mode: An update of VAL will be transferred to C2CC.VAL when the next CNTR.VAL is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When C2CFG.CCACT equals PER_PULSE_WIDTH_MEAS then VAL contains the width of the low or high phase of the selected signal. This is specified by C2CFG.EDGE. |
TGTNC is shown in Table 12-133.
Return to the Summary Table.
Target No Clear
Use this register to read or write to TGT without clearing the RIS.ZERO and RIS.TGT interrupt.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | FFFFh | User defined counter target value. |
C0CCNC is shown in Table 12-134.
Return to the Summary Table.
Channel 0 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C0CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C0CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C0CFG.CCACT determines if VAL is a signal period or a regular capture value. |
C1CCNC is shown in Table 12-135.
Return to the Summary Table.
Channel 1 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C1CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C1CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C1CFG.CCACT determines if VAL is a signal period or a regular capture value. |
C2CCNC is shown in Table 12-136.
Return to the Summary Table.
Channel 2 Capture Compare No Clear
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VAL | R/W | 0h | Capture Compare value. User defined compare value or channel-updated capture value. A read or write to this register will not clear the RIS.C2CC interrupt. Compare mode: VAL is compared against CNTR.VAL and an event is generated as specified by C2CFG.CCACT when these are equal. Capture mode: The current counter value is stored in VAL when a capture event occurs. C2CFG.CCACT determines if VAL is a signal period or a regular capture value. |