SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
Controlled power conversion between AC and DC is achieved by synchronizing the control unit with the grid frequency, achieving controlled amplitude and phase of the currents drained by the grid. To get the MCU synchronized with the grid, grid voltages (V_L1_A, V_L2_A, V_L3_A) are sampled by the MCU and fed to a phase-locked loop (PLL)11. By using the outcomes of the PLL (cos(φ), sin(φ)), plus Clarke and Park transforms, the three-phase system can be controlled by using the rotating frame reference technique (dq frame control), which allows the control to be simplified and improved.
Figure 77 is a schematic representation of the current control loop implemented in an AC/DC by using the rotating frame where measured Id and Iq can be derived by applying the Clarke and Park transformation to either I_L1_A, I_L2_A, I_L3_A or I_L1_B, I_L2_B, I_L3_B.
Figure 77 illustrates that the currents can be controlled by means of two PI controllers:
In addition to the PI controllers, feedforwards (FFW) are typically implemented in the current loops to decrease the response time and remove dependencies of the control loop bandwidths when variables in the system change (for example, if V_DC is not compensated, when V_DC decreases, control loop bandwidth can increase causing possible instabilities).