SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
To evaluate the minimum bandwidth required of a current sensor located in position D, when used for feedforward, system simulations were executed by applying the following conditions:
Simulations were performed to compare load transient performance with and without feedforward. Figure 92 shows the results. Without feedforward, the DC-link voltage drops significantly when the load is applied, leading to possible unstable converter operation. With feedforward, performance is drastically improved and the load transient response is reduced by a factor of 5. Conversely, the simulation results show how this additional sensor, in addition to the possibility to measure the power on the DC rail, is very useful when deployed with the load which connects and disconnects without giving a warning.
Figure 93 shows that the bandwidth of the current sensor only plays a minor role in the performance improvement since the overall bandwidth is limited by the dq current loop.
In summary, when placing a current sensor in point D for feedforward purposes, a low bandwidth of < 10 kHz is sufficient. In general, the bandwidth of the current sensor needs to be at least two times higher than the bandwidth of the current loop.