SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
To evaluate the impact of the gain error of a current sensor on the performance of the feedforward, simulations were performed for the following operating condition:
As Figure 94 shows, with an increment in the gain error in point D has only deteriorate slightly. This demonstrates that gain error is not a critical parameter when considering feedforward applications.
In summary, gain error in the DC-link current sensor has a minor effect on the overall transient load-step performance and gain errors up to 3% still achieve acceptable performance.