SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
A calculation tool was developed for simulation and validation purposes of the digital interface timings between an MCU and isolated Delta-Sigma modulators. The most common used isolated Delta-Sigma modulators AMC1306M25 and AMC1305L25 were selected for the digital interface timing analysis. AMC1305L25 has a LVDS interface type and requires LVDS driver and LVDS receiver when interfacing a MCU with CMOS interface. The MCU can be individually selected by the user, as only the setup and hold time requirements are entered into the calculation tool. In the following use of the calculation tool for the optimization of the digital interface timing between AMC1305L25 and C2000 MCU TMS320F28379D is shown step by step.