SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
Clock Signal Compensation by Clock Return is shown in Figure 3-4. With this compensation method, the clock signal that is fed into CLKIN the clock input of the AMC1306M25, is routed back from the CLKIN Pin of the AMC1306M25 to the SDFM clock input SDFM_CLKIN of the MCU.
By using this method, the same propagation delay by the clock buffer and the propagation delay introduced by the PCB trace length is achieved for the clock and data signal. Therefore, these delays in the clock and data signals cancel each other out.
However, the AMC1306M25 digital interface timing for data hold time th(MIN) = 3.5 ns and data delay time td (MAX) = 15 ns remains. This means that the timing needs to be checked after the PCB has been built to verify that the setup and hold timing requirements of the MCU for the SDFM are met. This type of compensation method is only recommended for isolated Delta-Sigma modulator with external clock source and CMOS interface.