SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
| ISO224 Input Voltage | ISO224 Output (VOUTP – VOUTN) | ADS7142 Input (Pseudo-Differential) | ADS7142 Digital Output |
|---|---|---|---|
| 12V | 4V | 3.3V | FFFH |
| –12V | –4V | 0V | 000H |
| Power Supplies and Reference Voltages | |||
|---|---|---|---|
| VDD1 | VDD2 and Vcc | AVDD | GND |
| 4.5V - 18V | 5V | 3.3V | 0V |
This circuit performs a ±12V isolated voltage sensing measurement using the ISO224 isolated amplifier, TLV9002 operational amplifier, and the ADS7142 SAR ADC. The ISO224 can measure single-ended signals of ±12V with a fixed gain of ⅓V/V and produces a ±4V isolated differential output voltage with an output common-mode voltage of VDD2 / 2. Channel 1 of the TLV9002 conditions the output of the ISO224 to fit the input range of the ADS7142, while channel 2 monitors the ISO224 fail-safe output. The ADS7142 is a dual-channel ADC with a full-scale input and reference voltage of AVDD which can range from 1.65V to 3.6V. For this cookbook circuit, the ADS7142 dual-channel input is used in a pseudo-differential configuration which allows for both positive and negative signals to be measured by the ISO224. This circuit is applicable to many high voltage industrial applications, such as Train Control and Management Systems, Analog Input Modules, and Inverter and Motor Control. The equations and explanation of component selection in this design can be customized based on system specifications and requirements.
| Specification | Calculated | Simulated |
|---|---|---|
| Transient ADC input settling at 140kSPS | 403µV | 88µV |
| Conditioned signal range | 0V–3.3V | 0V–3.3V |
| Noise (at the input) | 262µVRMS | 526µVRMS |
| Closed-loop bandwidth | 175kHz | 145kHz |
The ISO224 power supplies can be 4.5V to 18V for the high-side power supply, and 4.5V to 5.5V for the low-side power supply. The ISO224 has a ±12V single-ended input range with a fixed gain of ⅓V/V, yielding a ±4V differential output at a common-mode voltage of VDD2 / 2, 2.5V for this example:
The ADS7142 is a small sized, low power, dual channel ADC that can be used in a pseudo-differential configuration. The maximum input range is set by the reference voltage and is equal to AVDD, 3.3V for this example:
Find the required ADC common-mode voltage for pseudo-differential measurements:
The TLV9002 is a 2 channel, rail-to-rail input and output amplifier optimized for cost sensitive and small size applications.
Channel 1 is used to convert the ±4V differential, 2.5V common-mode output of the ISO224 to a 3.3V peak pseudo-differential output with a common-mode voltage of 1.65V. When R1 = R4 and R2 = R3, the transfer function is set by the following equation:
The signal must be converted from ±4V to 3.3V, this means that the signal must be reduced by a factor of 3.3V / ±4V = 3.3V / 8V. Substituting VCM with the previously calculated value of 1.65V and setting R2 and R3 to 10kΩ yields the following equations:
Solving for R1 and R4 yields values of 4.125kΩ.
Additional information on this topic can be seen in the Interfacing a Differential-Output (Isolated) Amplifier to a Single-Ended Input ADC application brief.
Channel 2 of the TLV9002 is used to monitor the fail-safe output feature of the ISO224. The ISO224 fail-safe output feature becomes active whenever the high-side power supply (VDD1) is missing independent of the input signal on the VIN pin. The TLV9002 channel 2 output (VCOMP) is fed to a GPIO port on the system controller and goes high whenever the fail-safe output feature is active. For additional details, see the Fail-Safe Output Feature application note.
Refine the RFILT and CFILT Values is a TI Precision Labs video showing the methodology for selecting RFILT and CFILT. The final value of 1.1kΩ and 330pF proved to settle to well below ½ of a least significant bit (LSB) within the acquisition window.
The following graphs show the simulated inputs of the TLV9002 and the ADS7142 from a ±15V input signal to the ISO224. The ISO224 has a linear output of ±VIN / 3 and the input to the TLV9002 can be seen in the first graph. The second graph shows that the TLV9002 further reduces the gain by VIN / 2.43 and shifts the common mode to 1.65V. This results in the full-range ±12V input signal using the 0V – 3.3V full-scale range (FSR) of the ADC with AVDD = VREF = 3.3V.
The following transfer function shows that the gain of the ISO224 and TLV9002 is 1/7.28V/V.
The simulated bandwidth of the signal chain is approximately 145kHz and the gain is –17.25dB, which is a linear gain of approximately 0.137V/V (attenuation ratio 1/7.28V/V). This matches the expected gain of the system.
The following simulation shows the transient settling results with an acquisition time of 5.3μs. The 88μV of noise is well within the 0.5 × LSB limit of 403μV. See Refine the Rfilt and Cfilt Values for detailed theory on this subject.
The simulated noise seen at the input of the ADC is greater than the expected calculated noise. This difference is due to noise peaking in the simulation model which is not included in the calculation. The following equations show that the ISO224 noise dominates the signal chain, and that the noise from the TLV9002 is negligible. See Calculating the Total Noise for ADC Systems for detailed theory on this subject.
See Analog Engineer's Circuit Cookbooks for TI's comprehensive circuit library.
TINA files for Isolated Design: SBAC226.
| Device | Key Features | Link | Similar Devices |
|---|---|---|---|
| ISO224 | ±12V single-ended input range, fixed gain of ⅓, yielding ±4V differential output, output common-mode voltage of 2.5V, 4.5V to 18V high-side power supply, 4.5V to 5.5V low side power supply, input offset: ±5mV at 25°C, ±42µV/°C maximum, gain error: ±0.3% at 25°C, ±50ppm/°C maximum, nonlinearity: ±0.01% maximum, ±1ppm/°C, high-input impedance of 1.25MΩ. | ISO224 | www.ti.com/isoamps |
| ADS7142 | Dual-channel, full-scale input span and reference set by AVDD, 12-bit performance by default, 16-bit performance with high precision mode, very low current consumption of 0.45µA at 600SPS. | ADS7142 | https://www.ti.com/PrecisionADCs |
| TLV9002 | Dual-channel, rail-to-rail input and output amplifier, low broadband noise of 2727nV/√ Hz, low input offset voltage of ±0.04mV. | TLV9002 | https://www.ti.com/opamps |