SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The INTxCONT bits in the ADCINTSEL1N2 and ADCINTSEL3N4 registers configure how interrupts are handled when an ADCINTFLG has not yet been cleared from a prior interrupt. This mode is disabled by default and additional overlapping interrupts are not issued to the Interrupt Controller. By activating this mode, ADC interrupts always reach the Interrupt Controller. If interrupts occur while ADCINTFLG is set, the ADCINTOVF register remains set regardless of the configuration of the INTxCONT bits.