The programming sequence is identical when using
the SEC units, regardless of whether the debug software or the application is
programing the units. Typical programming sequence for a unit is:
- Read and make sure the
ownership is set as expected. If not, acquire the ownership before
proceeding further if required.
- Make sure the unit is in IDLE
mode.
- Set up the counter reference,
counter registers (clear/reset if a clean start is required).
- Enable the corresponding
module bit in the enable register.
- Once the usage is completed,
write 1 to clear the EVENT_FIRED sticky bit. This takes the module back to
the enabled state.
Set up a free running counter:
- Read and make sure the
ownership is set as expected. If not, acquire the ownership before
proceeding further, if required.
- Read SEC_STATUS to confirm
that the module is in IDLE state.
- Write 0x0 to
CNT_INP_SEL_EN.
- Write 0x0 to SEC_CNTL.
- Enable the module in the
SEC_CNTL.EN register.
Set up the counter to count the duration spent
between addresses 0x1000 and 0x1210:
- Read and make sure the
ownership is set as expected. If not, acquire the ownership before
proceeding further, if required.
- Read SEC_STATUS to confirm
that the module is in IDLE state.
- Set up the EBC unit 1 to
generate an event for VPC = 0x1000.
- Set up the EBC unit 2 to
generate an event for VPC = 0x1210.
- Enable the module in the
SEC_CNTL.EN register.
Set up the counter to count the number of times a
function at address 0x2010 is called and fire an interrupt if this count reaches
0x300:
- Read and make sure the
ownership is set as expected. If not, acquire the ownership before
proceeding further, if required.
- Read SEC_STATUS to confirm
that the module is in IDLE state.
- Set up the EBC unit 1 to
generate an event for VPC = 0x2010.
- Write 0x300 SEC_REF.
- Enable the counter in the
EDGE_LEVEL, and also allow the counter to generate an interrupt when the
count matches the reference. This is achieved by writing 0x42 to
SEC_CNTL.
- Enable the module in the
SEC_CNTL.EN register.