SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
If parity is enabled, an ID parity error (PE) is detected if any of the two parity bits of the sent ID byte are not equal to the calculated parity on the receiver node. The two parity bits are generated using the following mixed parity algorithm:

If an ID-parity error is detected, the ID-parity error is flagged, and the received ID is not valid. See Section 40.3.1.9 for details.