SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
An SDRAM device requires that each of the rows be refreshed at a minimum required rate. The EMIF can meet this constraint by performing auto refresh cycles at or above this required rate. An auto-refresh cycle consists of issuing a PRE command to all banks of the SDRAM device followed by issuing a REFR command. To inform the EMIF of the required rate for performing auto refresh cycles, the RR field of the SDRAM refresh control register (SDRAM_RCR) must be programmed. The EMIF uses this value along with two internal counters to automatically perform auto refresh cycles at the required rate. The auto-refresh cycles cannot be disabled, even if the EMIF is not interfaced with an SDRAM. The remainder of this section details the EMIF's refresh scheme and provides an example for determining the appropriate value to place in the RR field of the SDRAM_RCR.
The two counters used to perform auto-refresh cycles are a 13-bit refresh interval counter and a 4-bit refresh backlog counter. At reset and upon writing to the RR field, the refresh interval counter is loaded with the value from RR field and begins decrementing, by one, each EMIF clock cycle. When the refresh interval counter reaches zero, the following actions occur:
The refresh backlog counter records the number of auto refresh cycles that the EMIF currently has outstanding. This counter is decremented by one each time an auto refresh cycle is performed and incremented by one each time the refresh interval counter expires. The refresh backlog counter saturates at the values of 0000b and 1111b. The EMIF uses the refresh backlog counter to determine the urgency with which an auto refresh cycle must be performed. The four levels of urgency are described in Table 14-13. This refresh scheme allows the required refreshes to be performed with minimal impact on access requests.
| Urgency Level | Refresh Backlog Counter Range | Action Taken |
|---|---|---|
| Refresh May | 1-3 | An auto-refresh cycle is performed only if the EMIF has no requests pending and none of the SDRAM banks are open. |
| Refresh Release | 4-7 | An auto-refresh cycle is performed if the EMIF has no requests pending, regardless of whether any SDRAM banks are open. |
| Refresh Need | 8-11 | An auto-refresh cycle is performed at the completion of the current access unless there are read requests pending. |
| Refresh Must | 12-15 | Multiple auto-refresh cycles are performed at the completion of the current access until the Refresh Release urgency level is reached. At that point, the EMIF can begin servicing any new read or write requests. |