SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
As PWM generation logic gets more configurable and the interaction between multiple PWM instances increases, there is potential for corner cases during applications resulting in unintended PWM states. To detect and make sure that under no circumstance, the PWM states result in potentially hazardous combinations, a Look Up Table (LUT) has been added. By default, the LUT logic is bypassed, LUTXTLx[BYPASS]. When not bypassed, based on the combination of values on Input 3 (IN3), Input 2 (IN2), and Input 1 (IN1), the value driven on OUT is determined by the bits in the LUTCTLx [23:16] register. Input 3 into the LUT comes from one of the ICL X-BAR inputs.