SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The voltage reference mode must be configured by using the ADC_setVREF() function, depending on the header files used, provided in C2000Ware. Using either of these functions makes sure that the correct trim is loaded in the ADC trim registers. This function must be called at least once after a device reset. Do not configure the voltage reference mode by directly writing to the ANAREFCTL register.