SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The Get Indices of the two Rx FIFOs (Rx FIFO 0 or Rx FIFO 1) and the Tx Event FIFO are controlled by writing to the corresponding FIFO Acknowledge Index (see MCAN_RXF0A, MCAN_RXF1A, and MCAN_TXEFA). Writing to the FIFO Acknowledge Index sets the FIFO Get Index to the FIFO Acknowledge Index plus one and, thereby, updates the FIFO Fill Level.
There are two use cases:
The Host CPU has free access to the Message RAM. Special care has to be taken when reading FIFO elements in an arbitrary order (Get Index not considered). This can be useful when reading a High Priority Message from one of the two Rx FIFOs. In this case, the FIFO Acknowledge Index must not be written because this sets the Get Index to a wrong position and also changes the FIFO's Fill Level. In this case, some of the older FIFO elements can be lost.