14 Revision History
Changes from September 30, 2024 to August 31, 2025 (from Revision E (September 2024) to Revision F (August 2025))
- Updated Common Platform Time Sync Module value in Modules Allocation
and Instances within Device Domains table.Go
- Added TOG Timeout Gasket chapter.Go
- Added Footnote to POST Selection table.Go
- Updated Serial NAND Boot Parameter TableGo
- Updated Clock Mapping table.Go
- Added Resets, Interrupts, and Clocks sections.Go
- Added LBIST Integration section.Go
- Added PVU Parameters section.Go
- Added PBIST Integration section.Go
- Added Timeout Gasket (TOG) section.Go
- MTOG Instances and Registers table and STOG Self-Test Target
Addresses and Self-Test Timeout Values table moved into Timeout Gasket (TOG)
Integration Details section.Go
- Added Safety Event Mapping for Compute Cluster (ESM Events)
section.Go
- Added R5FSS Not Supported Features section.Go
- Added Note to R5FSS ECC Support section.Go
- Updated Unsupported Features section.Go
- Added VPAC Not Supported Features section.Go
- Added LDC Not Supported Features section.Go
- Added MSC Not Supported Features section.Go
- Added DMPAC Not Supported Features section.Go
- Added Mailbox Not Supported Features section.Go
- Added Spinlock Not Supported Features section.Go
- Added DDRSS Not Supported Features section.Go
- Updated DDRSS Not Supported Features sectionGo
- Added PVU Integration section.Go
- Added PVU Not Supported Features section.Go
- Updated Interrupt Architecture section.Go
- Updated INTRTR Overview section.Go
- Added RINGACC Not Supported Features section.Go
- Added Proxy Not Supported Features section.Go
- Added Secure Proxy Not Supported Features section.Go
- Added CPTS Not Supported Features section.Go
- Added Timer Manager Not Supported Features section.Go
- Added ADC Not Supported Features section.Go
- ADC: Replaced registers with more generic names Go
- Updated AFE Functional Block DiagramGo
- Added GPIO Not Supported Features section.Go
- [Trigger
Configuration (per Bit)] updated method to return the value of the FAL_TRIG register. User
can read SET_FAL_TRIG or CLR_FAL_TRIG registers to obtain FAL_TRIG value (rather
than SET_FAL_TRIG and CLR_FAL_TRIG). Go
- Added I2C Not Supported Features section.Go
- Added I3C Not Supported Features section.Go
- Added MCSPI Not Supported Features section.Go
- [Peripheral Receive-Only Mode] Added clarification to definition of
full-duplex mode (requires 2 serial data lines).Go
- Added UART Not Supported Features section.Go
- Deleted the first paragraph for AM26x Devices as there is no
reference to the UART hardware requests that is mentioned in the first
paragraphGo
- Added PCIe Not Supported Features section.Go
- Added USB Not Supported Features section.Go
- Added SerDes Not Supported Features section.Go
- Added FSS Not Supported Features section.Go
- Added OSPI Not Supported Features
section.Go
- Added HyperBus Not Supported
Features section.Go
- Added GPMC Not Supported Features section.Go
- Added ELM Not Supported Features section.Go
- Added MMCSD Not Supported Features section.Go
- Added EPWM Not Supported Features section.Go
- Added EQEP Not Supported Features
section.Go
- Added MCAN Not Supported Features section.Go
- Added ATL Not Supported Features section.Go
- Added MCASP Not Supported Features section.Go
- Updated MCASP Module Block DiagramGo
- Added DSS Not Supported Features section.Go
- Added CSI_RX_IF Not Supported Features section.Go
- Added DPHY_RX Not Supported Features section.Go
- Added GTC Not Supported Features section.Go
- Added RTI Not Supported Features section.Go
- Added Timers Not Supported Features section.Go
- Added DCC Not Supported Features section.Go
- Added MCRC Not Supported Features section.Go
- Added Logical Built-In Self-Test (LBIST) chapter.Go
- Added Programmable Built-In Self Test (PBIST)
section.Go