SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
This section defines basic sequence flow chart divided into several sub sequences.
This section is applicable for MMCSD0 and MMCSD1 but MMCSD0 registers are used in the content.
UHSII is not supported. For more information, see Not Supported Features.
"Wait for interrupts" is used in the flow chart. This means the Host Driver waits until specified interrupts are asserted. If already asserted, then fall through that step in the flow chart. Timeout checking shall be always required to detect no interrupt generated but this is not described in the flow chart.
This specification uses the double box like Figure 12-120, (the step (1) in Figure 12-124), it means that the other flows, which already are shown, shall be performed. Therefore, the interrupt may be included in the other flows.
Figure 12-120 Double Box Notation