SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
There are two options after Self-Test operation has completed. If the IP module is not needed by the system, the software may leave the IP in the PSC disable state with no further action. If software desires to begin using the IP after Self-Test, the following operations must be performed: Software must restore system control of the block by: