SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The MSC module replicates missing lines and pixels at top/bottom and left/right sides of the input frame for non-interleaved (luma) and interleaved (chroma) data.
The missing lines at the top/bottom are replicated in the LSE sub-module prior to the vertical scaler and the missing pixels at the left/right sides of each line are replicated in the core prior to the horizontal scaler. For more information about LSE module, see Load Store Engine (LSE).
Replication scheme simply repeats the edge line or pixel to create missing lines/pixels. Figure 6-149 shows horizontal pixel replication.
Figure 6-149 Horizontal Pixel ReplicationIf a scaling is performed on a sub-frame (ROI) within the input frame, no replicated lines/pixels will be used since the lines/pixels outside the sub-frame are already present in the input frame.
For interleaved data format, the horizontal replication is done separately for U and V data. For U-data, edge U-pixel will be replicated. For V-data, edge V-pixel will be replicated. There is no distinction in the vertical edge padding.