SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Most digital cameras suffer from some degree of nonlinear geometric distortion. A spatial transformation is required to correct the distortion. In automotive applications, cameras use wide angle lenses, including fisheye lenses to provide 180+° field of view. To visually present the scene to the user in an easy-to-consume representation, these distortions need to be corrected
Back mapping gives coordinates of the distorted image as a function of coordinates of the undistorted output image. Correction involves back-mapping each output pixel to a location in the source distorted image, and thus the corrected image is fully populated. As the distorted pixel locations mostly fall onto fractional coordinates, correction involves interpolation.
As shown in Figure 6-125, the LDC consists of a back mapping block, a x/y offset table, image buffer interface, buffer, an interpolation block, and SL2 interface.
Figure 6-125 is a block diagram of the LDC.
Figure 6-125 LDC Block DiagramGiven the coordinates of the undistorted image, the corresponding coordinates of the distorted image are calculated by combining the output coordinates and the offsets from the offset table. Distorted pixels are read from the image buffer, and buffered for the bilinear interpolation. After the interpolation, corrected image is written back to the SL2 memory.
The LDC processes the image in small two-dimensional (2D) blocks. The software configures appropriate parameters, then initiates the LDC function by writing to an LDC register. The LDC controls the sequencing through 2D blocks, DMA transfers, and computation to process an entire image autonomously. Interrupt, if enabled, is asserted at the completion of the image.
The LDC write is controlled by HTS at block level.
To start the LDC, software must set the VPAC_LDC_CTRL[0] LDC_EN bit to 1. The VPAC_LDC_CTRL[2] BUSY bit is a status that reflects LDC activity.