SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The master interface on the bridge is the destination VBUSM port to send commands and receive data and status. These ports have the defined prefix, ss (SoC Slave, output of bridge), to identify them.
It is important to note that any feature not supported in the optional signals for this bus that is supported on the VBUSM.C interface will not be corrected inside the bridge. Examples are excluding the emudbg pin on this bus but expecting VBUSM.C transactions with emudbg set to not create bus status errors on this VBUSM bus outside the bridge (as the bridge will just pass the returned status which could be an error if it does not support the emudbg pin).