SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
All the parity inputs on the PCIe controller core are driven by the EDC_INV module. This allows the parity input to the PCIe controller to be inverted and thus inject an error. Figure 12-75 shows the parity logic on the AXI AWADDR port as an example. The parity of the AWADDR inputs to the PCIe controller are calculated as an XOR and this is fed into the PCIe controller using the EDC_INV block. The input AWADDR_par can be inverted using commands from the ECC Aggregator to enable error injection. Similar logic is present on all other parity inputs to the PCIe controller.
Checking input parity and output parity are handled inside the PCIe controller. Any errors in parity are signaled using the PCIe active internal diagnostics interrupt (PCIE_ASF_PEND).
Figure 12-75 Parity Logic on AXI AWADDR Input